STM32F4: OSC_OUT as GPIO when HSE in Bypass mode
ST moderator: post split from this thread.
Hello mƎALLEm,
Thank you for your confirmation on this issue.
I would like to provide some additional information. I have also encountered the same problem on the STM32F405RGT6.
In STM32CubeMX, when I configure both HSE or LSE to "Bypass Clock Source" mode, the tool insists on reserving PH1 (OSC_OUT) or PC15 (OSC32_OUT) as RCC pins. It blocks me from configuring them as regular GPIOs, even though the hardware (as you've confirmed) supports it.
Furthermore, I tested this on the STM32F446RE and STM32F446RC using the latest CubeMX, the problem still exists on those devices as well.
Regarding the internal tickets you mentioned (220390 for documentation, 222721 for CubeMX), may I kindly ask:
- Has the CubeMX fix (ticket 222721) been implemented in any release yet?
- If not, is there an estimated timeline for when we can expect this fix?
I understand if you cannot share internal details, but any update would be very helpful for our planning.
Thank you very much for your help, and sorry for my English as I'm not a native speaker.