Skip to main content
dingzeze0610
Associate
October 4, 2015
Question

stm32f4 IAP-how to produce a bin file for IAP programme

  • October 4, 2015
  • 1 reply
  • 725 views
Posted on October 04, 2015 at 04:00

Hello,

I'm using stm32f4 discovery board. The IDE I'm using is IAR EWARM. I have tried the sample code for IAP. But i want load my own code/program into the flash memory. So how i can produce a bin file which can be used for the IAP programme? 

#stm32f4 #iap #discovery
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
October 4, 2015
Posted on October 04, 2015 at 04:22

The goal is to generate a .BIN image for a firmware that resides at 0x08008000

I don't use IAR, but you should at the least be able to generate a .HEX file, from there you can use tools like HEX2BIN or SRECORD to generate a .BIN. IAR might have it's own tools to do this, or a check box, you'll have to read your documentation.

Other IAP examples for the F4 (USART, ETHERNET) might have additional examples of the ''app'' build methods/process. But it's basically to change the build address, and adjust the vector table (SCB->VTOR) settings in SystemInit(), et al, in system_stm32f4xx.c

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..