Skip to main content
c_m_87
Visitor II
November 24, 2013
Question

stm32f4 discovery / stm32-mat/target

  • November 24, 2013
  • 1 reply
  • 553 views
Posted on November 24, 2013 at 12:36

Hello,

I am trying to get my stm32f4 discovery working with the Matlab/Simulink package provided by ST.

I am currently using Matlab R2013a on Windows 8.

I am using Keil �Vision 5 as toolchain.

At the moment I am trying to get an LED blinking. So I am using two blocks the GPIOD_Config and the GPIO_Write.

But when I am building the model I get the following errors:

♯♯&sharpMakefile for KEIL

♯♯&sharpBuildMode : real_time MODELREF_TARGET_TYPE=NONE SIMULATION_MODE_RP=NO_PIL MAKEFILEBUILDER_TGT=0 STANDALONE_SUPPRESS_EXE=0

♯♯&sharpStartup file: startup_stm32f4xx.o  

♯♯&sharpStartup path: ''D:\Benutzer\much1021\Documents\STMicroelectronics\STM32F4xx''\lib\CMSIS\Device\ST\STM32F4xx\Source\Templates\arm

♯♯♯ Start compile .c source main.c

''main.c'', line 41: Error:  &sharp20: identifier ''RT_MODEL_ledd13'' is undefined

  extern RT_MODEL_ledd13 *const ledd13_M;

         ^

''main.c'', line 72: Error:  &sharp132: expression must have pointer-to-struct-or-union type

      rtmSetErrorStatus(ledd13_M, ''Overrun'');

      ^

main.c: 0 warnings, 2 errors

gmake: *** [main.o] Error 1

♯♯♯ Real-Time Workshop build procedure for method: 'error

♯♯♯ Real-Time Workshop build procedure for model: 'ledd13' aborted due to an error.

>>

Has someone had this problem too or knows how to fix it?

Thank You!

I got an update on my topic:

I changed to Keil �Vision4 now it almost works fine.

But when I build my example �V4 only starts in debug mode.

Has anyone figured out how I can actually flash my processor?

#stm32 #discovery #mat/target
    This topic has been closed for replies.

    1 reply

    Nickname12840_O
    Associate
    November 25, 2013
    Posted on November 25, 2013 at 14:22

    Hi,

    µVision5 is not managed for this version.

    So, you will not be able to automatically load program when µVision5 starts.

    Nevertheless build should work.

    I think you clicked RUN button instead of BUILD button.

    RUN button is only for simulation and PIL.

    When you build application using peripherals library, you must click on BUILD button. 

    Best regards

    Pascal