STM32F4-Discovery EEPROM emulation demo does not work
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-06 6:21 PM
I have STM32F4-Discovery board. (MB997B with Discovery-MO expansion board)
From STM32Cube package, I ran several examples, applications and demo successfully. But EEPROM_Emulation application does not work well.
STM32Cube_FW_F4_V1.13.0\Projects\STM32F4-Discovery\Applications\EEPROM\EEPROM_Emulation
When I start program, LD4 is blinking, indicating error is occurred. I tracked step-by-step, so error occurred here.
--
EE_Init(void)
switch (PageStatus0)/* Page0 valid, Page1 receive */ /* Transfer the variable to the Page1 */ EepromStatus = EE_VerifyPageFullWriteVariable(VirtAddVarTab[VarIdx], DataVar); /* If program operation was failed, a Flash error code is returned */ if (EepromStatus != HAL_OK) { return EepromStatus; }main()
/* EEPROM Init */
if( EE_Init() != EE_OK) { Error_Handler(); }--
I tried this with EWARM 7.70 and SW4STM32 and the result are same.
I don't understand why it does not work. I changed nothing in the program. There seems no hardware configuration.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-07 1:30 AM
Hi
Kim.Hansuk
‌,I tested the EEMPROM application on STM32F4-Discovery (STM32F407xx devices) using MDK-ARM V5.17 and IAR embedded workbench 7.70, and it works as expected.
Please before using the application, ensure that dedicated sectors for EEPROM (FLASH_SECTOR_2 and FLASH_SECTOR_3) are erased to avoid a match with a valid page OPCODE.
STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Applications\EEPROM\EEPROM_Emulation
-Nesrine-
Ifmy suggestanswers your question, please mark it as correct.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-13 10:34 AM
Try the eeprom code at this link.
It has a fix in EE_VerifyPageFullyErased ()
The version of code in the distribution only erases PAGE0
The code at this link has the same exact version in the header, as the one I had I the distribution (STM32Cube_FW_F4_V1.13.0) that is wrong
******************************************************************************
* @file EEPROM/EEPROM_Emulation/src/eeprom.c * @author MCD Application Team * @version V1.0.1 * @date 29-January-2016 * @brief This file provides all the EEPROM emulation firmware functions.Same problem exists in STM (STM32Cube_FW_F4_V1.14.0)
since only the header of the file changed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-13 12:14 PM
In eeprom_init, the code is setup to erase both pages if they are both marked valid. But it doesn't work. It only erases page0 not page1
/* Erase both Page0 and Page1 and set Page0 as valid page */
FlashStatus = EE_Format();