2013-02-26 1:39 AM
2013-02-28 5:16 AM
Hello Ram,
In order to check if really the problem root cause is a kind of ''interference'' between the inputs, would it be possible to configure only input 1 and check if the result remains the same after a reset for example. If the count doesn't remain the same, probably there is a configuration issue. Curious to know the results... Best Regards, ST.MCUTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-03-01 8:31 PM
Hello sir,
I have already configured only one input and observed the same problem .code mentioned in first post is for single input only Please go through the SDADC settingsSDADC_Config().
.Thanks.Ram2013-03-04 7:33 AM
Crosstalk can occur if the input impedance (RAIN) is not low. You have a 1 K input impedance that requires a sampling time as stated in Data Sheet Table 66. What sampling time is being used ?
Cheers, Hal2013-03-05 10:32 PM
Thanks
Hal
,I have configured sampling time as 1.5Mhz.and Now I have put 10E input impedance replacing 1k..But problem still exits.2013-03-05 11:59 PM
How are pins 49 (SDADC ground) and 52 (SDADC VREF+) connected?
JW2013-03-13 3:28 AM
Hello JW,
Please see pdf attached for pin 49 and 52 connections. thanks. ________________ Attachments : CONTROLLER.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0o3&d=%2Fa%2F0X0000000bdr%2FwOBPfMD7.K1y.TkgYSL3gFXBv77gAg2sUAsRO9EkY94&asPdf=false2013-03-13 6:43 AM
That looks OK.
I have no more ideas, sorry... JW2013-05-14 9:51 AM
Hello Ram,
Back to this discussion after 2 months!! I hope the issue is already fixed. If not, we can check again. So, In the code, why do you have this sequence:
1.
SDADC_VREFSelect(SDADC_VREF_VREFINT2);
2.
Delay_SW(1000);
3.
SDADC_Cmd(SDADC1, ENABLE);
4.
....
5.
SDADC_Cmd(SDADC1, DISABLE);
6.
....
7.
SDADC_Cmd(SDADC1, ENABLE); I think only the 1st enable is needed.
Let me know please.
Best Regards,
ST.MCU
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-07-01 4:56 AM
Hello
I just want to say, that our custom board has similar issue. We are using 8 SDADC single ended channels for resistance measurements and 8 ADC channels for voltage measurements. ADC and SDADC channels share some of analog circuit, but we don't see this problem when voltage is applied. So I assume it comes from inside of STM SDADC.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.