Skip to main content
Visitor II
Feb 14, 2024 8:05 PM UTC
Question

STM32F3348-DISCO HRTIM DMA PWM Sine Wave

Hi all,

I wanted to make a post to shine some light on how to configure the HRTIM DMA on the STM32F3348-DISCO (and probably other ICs w/ HRTIM capabilities).

A few posts I've seen have boasted the same solution, but have convoluted the use of a single DMA request, Burst DMA requests and general Burst Mode configuration using the HRTIM. Here I'll try and walk through a step-by-step CubeMX and main.c configuration to step through a sine table with a circular DMA request to create a high frequency PWM sine wave using HRTIM1. Some basic knowledge of the ST Cube suite is assumed.

  1. Start a new CubeMX project - Select "Start My Project from ST Board" --> Search "STM32F3348-DISCO" --> Select board and "Start Project" (initialize peripherals in default mode).
  2. In Timers -> HRTIM1: disable Timer C (this example we'll only use Timer D) 
  3. In Timers -> HRTIM1 -> DMA Settings: Add HRTIM1_D and set:
    • DMA_Settings.png
    • Direction = Memory to Peripheral
    • Priority = High
    • Mode = Circular
    • Data Width = Word
  4. In Timers -> HRTIM1 -> Timer D: Only change the following settings, leave the rest unchanged. Some settings will be set in Cube IDE.
    • Timing Unit -> Preload Enable = Preload Enabled
    • Timing Unit -> Number of Timer D Internal DMA Request.. = 1
    • Timing Unit -> Number of Timer D Internal DMA Request.. -> 1st DMA Request Source = Timer repetition DMA request enable
    • Timing Unit -> DMA Src Address = (uint32_t)&signal[0]
    • Timing Unit -> DMA Dst Address = (uint32_t)&(hhrtim1).Instance->sTimerxRegs[(HRTIM_TIMERINDEX_TIMER_D)].CMP1xR
    • Compare Unit 1 -> Compare Unit 1 Configuration = Enable
    • Output 1 Configuration -> Set Source Selection = 1
    • Output 1 Configuration -> Set Source Selection -> 1st Set Source = Timer period event forces the output..
    • Output 1 Configuration -> Reset Source Selection = 1
    • Output 1 Configuration -> Reset Source Selection -> 1st Set Source = Timer compare 1 event forces the output..
  5. Generate your code into STM32CubeIDE (need to change default toolchain in Project Manager tab).
  6. Copy and paste the contents of the attached main.c file. The important things are: 
    1. Sine lookup table is pre-generated and stored in uint32_t array "signal" of size "NS". 
    2. HAL_HRTIM_WaveformOutputStart is called first inside main function, then HAL_HRTIM_WaveformCountStart_DMA.
    3. Inside MX_HRTIM1_Init(): pTimeBaseCfg.Period = PERIOD; pTimerCfg.DMASize = NS;
  7. Debug as STM32 C/C++ Application (assuming board is connected properly).

Hooking an oscilloscope up to PB14 (on STM32F3348-DISCO) you should see a PWM wave with a frequency of 100kHz changing duty cycle rapidly. 

Hopefully this helps clarify some of the ambiguity of configuring the HRTIM. I'm excited to go further and sync some basic sampling with a few of the ADCs on the chip.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

//DEFINING THE NUMBER OF SAMPLES/STEPS IN SINE WAVE
#define NS		128

//DEFINING THE PERIOD OF THE PWM
#define PERIOD	46080	//100kHz

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
HRTIM_HandleTypeDef hhrtim1;
DMA_HandleTypeDef hdma_hrtim1_d;

/* USER CODE BEGIN PV */
uint32_t signal[NS] = {
 23040, 24171, 25298, 26421, 27535, 28638, 29728, 30802, 31857, 32891, 33901, 34885,
 35840, 36765, 37656, 38513, 39332, 40112, 40850, 41546, 42197, 42802, 43359, 43868,
 44326, 44733, 45088, 45390, 45637, 45831, 45969, 46052, 46080, 46052, 45969, 45831,
 45637, 45390, 45088, 44733, 44326, 43868, 43359, 42802, 42197, 41546, 40850, 40112,
 39332, 38513, 37656, 36765, 35840, 34885, 33901, 32891, 31857, 30802, 29728, 28638,
 27535, 26421, 25298, 24171, 23040, 21909, 20782, 19659, 18545, 17442, 16352, 15278,
 14223, 13189, 12179, 11195, 10240, 9315, 8424, 7567, 6748, 5968, 5230, 4534,
 3883, 3278, 2721, 2212, 1754, 1347, 992, 690, 443, 249, 111, 28,
 0, 28, 111, 249, 443, 690, 992, 1347, 1754, 2212, 2721, 3278,
 3883, 4534, 5230, 5968, 6748, 7567, 8424, 9315, 10240, 11195, 12179, 13189,
 14223, 15278, 16352, 17442, 18545, 19659, 20782, 21909}; 
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_HRTIM1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
	
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_HRTIM1_Init();
 /* USER CODE BEGIN 2 */

 //	STARTING WAVEFORM OUTPUT ON HRTIM D1 (PIN B14)
 HAL_HRTIM_WaveformOutputStart(&hhrtim1, HRTIM_OUTPUT_TD1);

 //	START HRTIM COUNTER + CIRCULAR DMA TRANSFER TO HRTIM D COMP1
 HAL_HRTIM_WaveformCountStart_DMA(&hhrtim1, HRTIM_TIMERID_TIMER_D);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_HRTIM1;
 PeriphClkInit.Hrtim1ClockSelection = RCC_HRTIM1CLK_PLLCLK;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief HRTIM1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_HRTIM1_Init(void)
{

 /* USER CODE BEGIN HRTIM1_Init 0 */

 /* USER CODE END HRTIM1_Init 0 */

 HRTIM_TimeBaseCfgTypeDef pTimeBaseCfg = {0};
 HRTIM_TimerCfgTypeDef pTimerCfg = {0};
 HRTIM_CompareCfgTypeDef pCompareCfg = {0};
 HRTIM_OutputCfgTypeDef pOutputCfg = {0};

 /* USER CODE BEGIN HRTIM1_Init 1 */

 /* USER CODE END HRTIM1_Init 1 */
 hhrtim1.Instance = HRTIM1;
 hhrtim1.Init.HRTIMInterruptResquests = HRTIM_IT_NONE;
 hhrtim1.Init.SyncOptions = HRTIM_SYNCOPTION_NONE;
 if (HAL_HRTIM_Init(&hhrtim1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_HRTIM_DLLCalibrationStart(&hhrtim1, HRTIM_CALIBRATIONRATE_14) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_HRTIM_PollForDLLCalibration(&hhrtim1, 10) != HAL_OK)
 {
 Error_Handler();
 }
 pTimeBaseCfg.Period = PERIOD;
 pTimeBaseCfg.RepetitionCounter = 0x00;
 pTimeBaseCfg.PrescalerRatio = HRTIM_PRESCALERRATIO_MUL32;
 pTimeBaseCfg.Mode = HRTIM_MODE_CONTINUOUS;
 if (HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, &pTimeBaseCfg) != HAL_OK)
 {
 Error_Handler();
 }
 pTimerCfg.InterruptRequests = HRTIM_TIM_IT_NONE;
 pTimerCfg.DMARequests = HRTIM_TIM_DMA_REP;
 pTimerCfg.DMASrcAddress = (uint32_t)&signal[0];
 pTimerCfg.DMADstAddress = (uint32_t)&(hhrtim1).Instance->sTimerxRegs[(HRTIM_TIMERINDEX_TIMER_D)].CMP1xR;
 pTimerCfg.DMASize = NS;
 pTimerCfg.HalfModeEnable = HRTIM_HALFMODE_DISABLED;
 pTimerCfg.StartOnSync = HRTIM_SYNCSTART_DISABLED;
 pTimerCfg.ResetOnSync = HRTIM_SYNCRESET_DISABLED;
 pTimerCfg.DACSynchro = HRTIM_DACSYNC_NONE;
 pTimerCfg.PreloadEnable = HRTIM_PRELOAD_ENABLED;
 pTimerCfg.UpdateGating = HRTIM_UPDATEGATING_INDEPENDENT;
 pTimerCfg.BurstMode = HRTIM_TIMERBURSTMODE_MAINTAINCLOCK;
 pTimerCfg.RepetitionUpdate = HRTIM_UPDATEONREPETITION_ENABLED;
 pTimerCfg.PushPull = HRTIM_TIMPUSHPULLMODE_DISABLED;
 pTimerCfg.FaultEnable = HRTIM_TIMFAULTENABLE_NONE;
 pTimerCfg.FaultLock = HRTIM_TIMFAULTLOCK_READWRITE;
 pTimerCfg.DeadTimeInsertion = HRTIM_TIMDEADTIMEINSERTION_DISABLED;
 pTimerCfg.DelayedProtectionMode = HRTIM_TIMER_D_E_DELAYEDPROTECTION_DISABLED;
 pTimerCfg.UpdateTrigger = HRTIM_TIMUPDATETRIGGER_NONE;
 pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_NONE;
 pTimerCfg.ResetUpdate = HRTIM_TIMUPDATEONRESET_DISABLED;
 if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, &pTimerCfg) != HAL_OK)
 {
 Error_Handler();
 }
 pCompareCfg.CompareValue = PERIOD/2;
 if (HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_COMPAREUNIT_1, &pCompareCfg) != HAL_OK)
 {
 Error_Handler();
 }
 pOutputCfg.Polarity = HRTIM_OUTPUTPOLARITY_HIGH;
 pOutputCfg.SetSource = HRTIM_OUTPUTSET_TIMPER;
 pOutputCfg.ResetSource = HRTIM_OUTPUTRESET_TIMCMP1;
 pOutputCfg.IdleMode = HRTIM_OUTPUTIDLEMODE_NONE;
 pOutputCfg.IdleLevel = HRTIM_OUTPUTIDLELEVEL_INACTIVE;
 pOutputCfg.FaultLevel = HRTIM_OUTPUTFAULTLEVEL_NONE;
 pOutputCfg.ChopperModeEnable = HRTIM_OUTPUTCHOPPERMODE_DISABLED;
 pOutputCfg.BurstModeEntryDelayed = HRTIM_OUTPUTBURSTMODEENTRY_REGULAR;
 if (HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_D, HRTIM_OUTPUT_TD1, &pOutputCfg) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN HRTIM1_Init 2 */

 /* USER CODE END HRTIM1_Init 2 */
 HAL_HRTIM_MspPostInit(&hhrtim1);

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel6_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel6_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel6_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, LD_U_Pin|LD_D_Pin|LD_L_Pin|LD_R_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : Vin_Sense_Pin Vout_Sense_Pin */
 GPIO_InitStruct.Pin = Vin_Sense_Pin|Vout_Sense_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : BK_Sense_Pin */
 GPIO_InitStruct.Pin = BK_Sense_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(BK_Sense_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : LD_U_Pin LD_D_Pin LD_L_Pin LD_R_Pin */
 GPIO_InitStruct.Pin = LD_U_Pin|LD_D_Pin|LD_L_Pin|LD_R_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
This topic has been closed for replies.

1 reply

Associate II
May 23, 2025 7:58 AM UTC

Hi Claude_Lou, 

I tried to configure HRTIM and implement like you but it'snot working.