Skip to main content
Jeck7778
Associate II
January 2, 2017
Solved

STM32F303K8 ADC Calibration phase problem

  • January 2, 2017
  • 4 replies
  • 1106 views
Posted on January 02, 2017 at 17:01

This is my CODE:

void ADC_t_init(void)

{

    ADC_InitTypeDef          ADC_InitStrc;

    ADC_CommonInitTypeDef     ADC_CmmInitStrc;

    /* Configure the ADC clock */

    RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div256);

    /* Enable ADC1 clock */

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);

    /* Calibration procedure */

    ADC_StructInit(&ADC_InitStrc);

    ADC_Init(ADC1, &ADC_InitStrc);

    ADC_Cmd(ADC1, DISABLE);

    ADC_VoltageRegulatorCmd(ADC1, ENABLE);

    /* Insert delay equal to 10 µs */

    Delay(10);

    ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);

    ADC_StartCalibration(ADC1);

    while(ADC_GetCalibrationStatus(ADC1));

    calibration_value = ADC_GetCalibrationValue(ADC1);

    ADC_CmmInitStrc.ADC_Mode                 = ADC_Mode_Independent;

    ADC_CmmInitStrc.ADC_Clock                 = ADC_Clock_AsynClkMode;

    ADC_CmmInitStrc.ADC_DMAAccessMode         = ADC_DMAAccessMode_Disabled;

    ADC_CmmInitStrc.ADC_DMAMode             = ADC_DMAMode_OneShot;

    ADC_CmmInitStrc.ADC_TwoSamplingDelay     = 0;

    ADC_CommonInit(ADC1, &ADC_CmmInitStrc);

    ADC_InitStrc.ADC_ContinuousConvMode     = ADC_ContinuousConvMode_Enable;

    ADC_InitStrc.ADC_Resolution             = ADC_Resolution_12b;

    ADC_InitStrc.ADC_ExternalTrigConvEvent     = ADC_ExternalTrigConvEvent_0;

    ADC_InitStrc.ADC_ExternalTrigEventEdge     = ADC_ExternalTrigEventEdge_None;

    ADC_InitStrc.ADC_DataAlign                 = ADC_DataAlign_Right;

    ADC_InitStrc.ADC_OverrunMode             = ADC_OverrunMode_Disable;

    ADC_InitStrc.ADC_AutoInjMode             = ADC_AutoInjec_Disable;

    ADC_InitStrc.ADC_NbrOfRegChannel         = 1;

    ADC_Init(ADC1, &ADC_InitStrc);

    /* ADC1 Temperature sensor configuration */

    ADC_RegularChannelConfig(ADC1, ADC_Channel_TempSensor, 1, ADC_SampleTime_601Cycles5);

    /* Enable ADC1 */

    ADC_Cmd(ADC1, ENABLE);

    /* Enable temperature sensor */

    ADC_TempSensorCmd(ADC1,ENABLE);

    /* wait for ADRDY */

    while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));

    /* Start ADC1 Software Conversion */

    ADC_StartConversion(ADC1);

}

and the program not exit from:

while(ADC_GetCalibrationStatus(ADC1));

anyone know where is the problem?

thenks for help.

    This topic has been closed for replies.
    Best answer by Khouloud GARSI
    Posted on January 10, 2017 at 10:32

    Hi

    Giacomo.Cimarelli

    ,

    - Theline 'ADC_Cmd(ADC1, DISABLE);' will set the ADDIS bit (ADDIS=1).

    Your ADC was never enabled before this line, so ADEN=0.

    - On the reference manual, it's indicated that :

    'Software is allowed to set ADDIS only when ADEN=1 and both ADSTART=0 and JADSTART=0

    (which ensures that no conversion is ongoing)'

    -> What you are trying to do is out of specification.

    What you should do is to comment the line below: 'ADC_Cmd(ADC1, DISABLE);'

    And your code will be executedconveniently.

    Khouloud.

    4 replies

    Khouloud GARSI
    ST Employee
    January 2, 2017
    Posted on January 02, 2017 at 17:40

    Hi

    Giacomo.Cimarelli

    ,

    You have disabled the

    ADC1 peripheral using: ADC_Cmd(ADC1, DISABLE);

    Try to enable it beforechecking the end of calibration.

    If this solves your issue, please click on correct

    :)

    .

    Happy new year .

    Khouloud.

    Jeck7778
    Jeck7778Author
    Associate II
    January 3, 2017
    Posted on January 03, 2017 at 00:33

    Hi

    Khouloud G

    .

    On the ST Reference Manual is written:

    The calibration is then initiated by software by setting bit ADCAL=1. Calibration can only be

    initiated when the ADC is disabled (when ADEN=0). ADCAL bit stays at 1 during all the

    calibration sequence. It is then cleared by hardware as soon the calibration completes. At

    this time, the associated calibration factor is stored internally in the analog ADC and also in

    the bits CALFACT_S[6:0] or CALFACT_D[6:0] of ADCx_CALFACT register (depending on

    single-ended or differential input calibration)

    For the calibration need kept ADC disabled right?

    I have try to enabling it but not work.

    Khouloud GARSI
    Khouloud GARSIBest answer
    ST Employee
    January 10, 2017
    Posted on January 10, 2017 at 10:32

    Hi

    Giacomo.Cimarelli

    ,

    - Theline 'ADC_Cmd(ADC1, DISABLE);' will set the ADDIS bit (ADDIS=1).

    Your ADC was never enabled before this line, so ADEN=0.

    - On the reference manual, it's indicated that :

    'Software is allowed to set ADDIS only when ADEN=1 and both ADSTART=0 and JADSTART=0

    (which ensures that no conversion is ongoing)'

    -> What you are trying to do is out of specification.

    What you should do is to comment the line below: 'ADC_Cmd(ADC1, DISABLE);'

    And your code will be executedconveniently.

    Khouloud.

    Jeck7778
    Jeck7778Author
    Associate II
    January 10, 2017
    Posted on January 10, 2017 at 12:56

    Thenks for the help now work!