cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F3 - what exactly are conditions and benefits of using FLASH half cycle access?

waclawek.jan
Super User

in RM0316 rev.8. FLASH_ACR.HLFCYA is described as enabling Flash half cycle access. Narrative in chapter 4.2.2 says:

If there is not any high frequency clock available in the system, Flash memory accesses can

be made on a half cycle of HCLK (AHB clock).

Besides a subsequent sentence which prohibits using half-cycle mode when AHB divider is non-1, I can't find any other reference to this mode, not in RM0316, not in DS, nowhere else.

Can please ST quantify "high frequency clock" in the quote above, and also explain/quantify what are the benefits of using this mode.

Thanks,

JW

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0