cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F2XX Ethernet IAP

Asantos
Senior
Posted on December 06, 2011 at 15:31

I've tested the F2xx IAP over ethernet and it didn't work for me, the communications works okay, but the flash erase routine doesn't  work.

    Has someone tested this application?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
amin23
Associate II
Posted on December 07, 2011 at 07:56

- check the STM32 EVAL jumpers setting

- which FW version you are using

- which protocol do you use http or tftp

Asantos
Senior
Posted on December 07, 2011 at 13:33

I'm using a custom board. I tried with both protocols. I noted that the erase flash function is called but it doesn't erase the flash.

This application worked for you?

amin23
Associate II
Posted on December 07, 2011 at 13:55

I am using ST EVAL, it works well.