2024-07-29 4:52 AM
I made a board with spi1 connect a lora module, and the nss pin, I just want to use soft control. But I found that before I enable spi1, the SPI CR1 and CR2 register value as:
(gdb) x/2wx 0x40013000
0x40013000: 0x00000024 0x00000040
but after I do spi_enable(SPI1), I get these register as below:
(gdb) x/2wx 0x40013000
0x40013000: 0x00000020 0x00000040
This is the releate codes:
spi_init_master(controller, SPI_CR1_BAUDRATE_FPCLK_DIV_32, SPI_CR1_CPOL_CLK_TO_0_WHEN_IDLE,
SPI_CR1_CPHA_CLK_TRANSITION_1, SPI_CR1_DFF_8BIT, SPI_CR1_MSBFIRST, SPI_NSS_SOFT);
spi_enable_rx_buffer_not_empty_interrupt(controller);
spi_enable(controller);
int spi_init_master(uint32_t spi, uint32_t br, uint32_t cpol, uint32_t cpha,
uint32_t dff, uint32_t lsbfirst, uint32_t nss)
{
uint32_t reg32 = SPI_CR1(spi);
/* Reset all bits omitting SPE, CRCEN and CRCNEXT bits. */
reg32 &= SPI_CR1_SPE | SPI_CR1_CRCEN | SPI_CR1_CRCNEXT;
reg32 |= SPI_CR1_MSTR; /* Configure SPI as master. */
reg32 |= br; /* Set baud rate bits. */
reg32 |= cpol; /* Set CPOL value. */
reg32 |= cpha; /* Set CPHA value. */
reg32 |= dff; /* Set data format (8 or 16 bits). */
reg32 |= lsbfirst; /* Set frame format (LSB- or MSB-first). */
/* reg32 |= nss & 0XFFFF; */
SPI_CR1(spi) = reg32;
if (nss == SPI_NSS_HARD_OUTPUT)
SPI_CR2(spi) |= SPI_CR2_SSOE; /* common case */
else
SPI_CR2(spi) &= ~SPI_CR2_SSOE; /* common case */
return 0;
}
void spi_enable_rx_buffer_not_empty_interrupt(uint32_t spi)
{
SPI_CR2(spi) |= SPI_CR2_RXNEIE;
}
void spi_enable(uint32_t spi)
{
SPI_CR1(spi) |= SPI_CR1_SPE; /* Enable SPI. */
}