cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f0discovery - problem with UART DMA transfer

krzysztof23
Associate II
Posted on March 06, 2015 at 14:21

Hi.

I am a newbe in STM32 microcontroles. I have problems with starting the DMA transfer to UART.

This is my init for UART.

/*

* Helpers for DMA configuration

*/

static UART_HandleTypeDef *hRS232_handle=&RS232_handle;

static DMA_HandleTypeDef RS232_RX_DMA_handle;

static DMA_HandleTypeDef RS232_TX_DMA_handle;

/*

* GPIO UART pin configuration

*/

/*

* GPIO Clock enable

*/

__GPIOA_CLK_ENABLE();

/*

* Configure GPIO RX & TX Pins.

* For UART2 TX - PA2

* For UART2 RX - PA3

*/

GPIO_InitTypeDef GPIO_InitStruct;

GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_3;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_PULLUP;

GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF1_USART2;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/*

* USART port clock enable

*/

__USART2_CLK_ENABLE();

/*

* Configure USART parameters

*/

RS232_handle.Instance = USART2;

RS232_handle.Init.BaudRate = 300;

RS232_handle.Init.WordLength = USART_WORDLENGTH_8B;

RS232_handle.Init.StopBits = USART_STOPBITS_1;

RS232_handle.Init.Parity = USART_PARITY_NONE;

RS232_handle.Init.Mode = USART_MODE_TX_RX;

RS232_handle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

/*

* Configure DMA Clock

*/

__DMA1_CLK_ENABLE();

/*

* Configure DMA RX Channel

*/

RS232_RX_DMA_handle.Instance = DMA1_Channel4;

RS232_RX_DMA_handle.Init.Direction = DMA_PERIPH_TO_MEMORY;

RS232_RX_DMA_handle.Init.PeriphInc = DMA_PINC_DISABLE;

RS232_RX_DMA_handle.Init.MemInc = DMA_MINC_ENABLE;

RS232_RX_DMA_handle.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

RS232_RX_DMA_handle.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;

RS232_RX_DMA_handle.Init.Mode = DMA_NORMAL;

RS232_RX_DMA_handle.Init.Priority = DMA_PRIORITY_LOW;

HAL_DMA_Init(&RS232_RX_DMA_handle);

__HAL_LINKDMA(hRS232_handle, hdmarx, RS232_RX_DMA_handle);

/*

* Interrupt for DMA TX channel.

*/

HAL_NVIC_SetPriority(DMA1_Channel4_5_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(DMA1_Channel4_5_IRQn);

/*

* Configure DMA TX Channel

*/

RS232_TX_DMA_handle.Instance = DMA1_Channel5;

RS232_TX_DMA_handle.Init.Direction = DMA_MEMORY_TO_PERIPH;

RS232_TX_DMA_handle.Init.PeriphInc = DMA_PINC_DISABLE;

RS232_TX_DMA_handle.Init.MemInc = DMA_MINC_ENABLE;

RS232_TX_DMA_handle.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

RS232_TX_DMA_handle.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;

RS232_TX_DMA_handle.Init.Mode = DMA_NORMAL;

RS232_TX_DMA_handle.Init.Priority = DMA_PRIORITY_HIGH;

HAL_DMA_Init(&RS232_TX_DMA_handle);

__HAL_LINKDMA(hRS232_handle, hdmatx, RS232_TX_DMA_handle);

/*

* Interrupt for DMA TX channel.

*/

HAL_NVIC_SetPriority(DMA1_Channel4_5_IRQn, 0, 1);

HAL_NVIC_EnableIRQ(DMA1_Channel4_5_IRQn);

/*

* Configure Interrupt for UART

*/

HAL_NVIC_SetPriority(USART2_IRQn, 0, 1);

HAL_NVIC_EnableIRQ(USART2_IRQn);

/*

* Initialize USART

*/

HAL_UART_Init(&RS232_handle);

For DMA IRQ:

void DMA1_Channel4_5_IRQHandler(void){

HAL_DMA_IRQHandler(RS232_handle.hdmatx);

HAL_DMA_IRQHandler(RS232_handle.hdmarx);

}

Everything works fine when I am using the Polling mode - HAL_UART_Transmit

But when I am trying to use HAL_UART_Transmit_DMA, I can not see any transfer form the UART. 

When I try to use breakpoint on IRQ, the breakpoint never stops the program.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
krzysztof23
Associate II
Posted on March 24, 2015 at 12:59

Solved. 

The DMA Channels has been mixed up.

For UART 2 TX the proper DMA Channel is 4

For UART 2 TX the proper DMA Channel is 5

krzysztof23
Associate II
Posted on March 24, 2015 at 13:00

Found it.

The DMA channels has been mixed up.

For UART 2 TX propper DMA channel is 4

For UART 2 RX propper DMA channel is 5.