Associate
November 3, 2016
Question
STM32F072 battery reading
- November 3, 2016
- 2 replies
- 1233 views
Posted on November 04, 2016 at 00:59
Hi All
I have the attached circuit and I need to read the battery level using ADC_IN18. I have the following instructions:Init:
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
ADC_Init(ADC1, &ADC_InitStructure);
///// other stuffs ///
ADC_AutoPowerOffCmd(ADC1, ENABLE);//Enables or disables the ADC Power Off.
ADC_VbatCmd(ENABLE);
/* Start ADC1 Software Conversion */
ADC_StartOfConversion(ADC1);
/* Wait until ADC end of conversion */
while (ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET) {}
/* Read ADC conversion result */
V_Value = ADC_GetConversionValue(ADC1);
I'm getting the value 2072 +/- 4
This value I'm getting whether the battery is charged or empty. Can someone help understand and solve it ? I'm not fw programmer, this just fall over me because our guy is sick and I need to deliver this project.Any help welcome.Thanks #battery #adc #stm32f072