Question
STM32F030F4Px USART problem
i'm using STM32F030F4Px for MODBUS Master Slave communication based on USART (RS485 communication). i'm using 9600 baud rate, 8bit 1 stop bit communication with DMA and HAL.
Master is transmitting 8 bytes to slave after 10 or 20 msec which are received at slave end perfectly.
However, when slave responds to master, the slave stops receiving data from master.