STM32F0 DMA communication
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-16 7:22 AM
Hi all,i want to STM32F0 DMA communication Peripheral to Perpheral.but when i debugging my codes,in my while loop code works one time and stops.What is my fault.My code is here;
/* Includes ------------------------------------------------------------------*/
#include ''stm32f0xx.h''
#include ''stm32f0xx_rcc.h''
#include ''stm32f0xx_gpio.h''
#include ''stm32f0xx_usart.h''
#include ''stm32f0xx_dma.h''
#include ''stm32f0xx_misc.h''
#include <
stdio.h
>
uint32_t DMA_Array[8];
/**************************************************************************************/
void RCC_Configuration(void)
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1ENR_USART2EN,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1,ENABLE);
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_Struct;
GPIO_InitTypeDef GPIO_Struct2;
GPIO_InitTypeDef GPIO_Struct3;
/*USART1 PA9-TX PA10-RX*/
GPIO_Struct.GPIO_Pin=((GPIO_Pin_9)|(GPIO_Pin_10));
GPIO_Struct.GPIO_Mode=GPIO_Mode_AF;
GPIO_Struct.GPIO_OType=GPIO_OType_PP;
GPIO_Struct.GPIO_PuPd=GPIO_PuPd_NOPULL;
GPIO_Struct.GPIO_Speed=GPIO_Speed_50MHz;
GPIO_Init(GPIOA,&GPIO_Struct);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
/*USART2 PA2-TX PA3-RX*/
GPIO_Struct2.GPIO_Pin=(GPIO_Pin_2)|(GPIO_Pin_3);
GPIO_Struct2.GPIO_Mode=GPIO_Mode_AF;
GPIO_Struct2.GPIO_OType=GPIO_OType_PP;
GPIO_Struct2.GPIO_PuPd=GPIO_PuPd_NOPULL;
GPIO_Struct2.GPIO_Speed=GPIO_Speed_50MHz;
GPIO_Init(GPIOA,&GPIO_Struct2);
GPIO_PinAFConfig(GPIOA,GPIO_PinSource2,GPIO_AF_1);
GPIO_PinAFConfig(GPIOA,GPIO_PinSource3,GPIO_AF_1);
}
void USARTs_Configuration(void)
{
USART_InitTypeDef USART_Struct;
USART_InitTypeDef USART_Struct2;
USART_Struct.USART_BaudRate=9600;
USART_Struct.USART_HardwareFlowControl=USART_HardwareFlowControl_None;
USART_Struct.USART_Mode=(USART_Mode_Rx|USART_Mode_Tx);
USART_Struct.USART_Parity=USART_Parity_No;
USART_Struct.USART_StopBits=USART_StopBits_1;
USART_Struct.USART_WordLength=USART_WordLength_8b;
USART_Init(USART1,&USART_Struct);
USART_Cmd(USART1,ENABLE);
USART_Struct2.USART_BaudRate=9600;
USART_Struct2.USART_HardwareFlowControl=USART_HardwareFlowControl_None;
USART_Struct2.USART_Mode=(USART_Mode_Rx|USART_Mode_Tx);
USART_Struct2.USART_Parity=USART_Parity_No;
USART_Struct2.USART_StopBits=USART_StopBits_1;
USART_Struct2.USART_WordLength=USART_WordLength_8b;
USART_Init(USART2,&USART_Struct2);
USART_Cmd(USART2,ENABLE);
}
void DMA_Configuration(void)
{
DMA_InitTypeDef DMA_Struct;
NVIC_InitTypeDef NVIC_Struct;
/***/
DMA_Struct.DMA_BufferSize = 8;
DMA_Struct.DMA_DIR=DMA_DIR_PeripheralSRC;
DMA_Struct.DMA_M2M = DMA_M2M_Enable;
DMA_Struct.DMA_MemoryBaseAddr=(uint32_t)&USART2->TDR;
DMA_Struct.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_Struct.DMA_PeripheralInc =DMA_PeripheralInc_Enable;
DMA_Struct.DMA_Mode = DMA_Mode_Circular;
DMA_Struct.DMA_PeripheralBaseAddr=(uint32_t)&USART1->RDR;
DMA_Struct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_Struct.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_Struct.DMA_Priority = DMA_Priority_High ;
DMA_ClearITPendingBit(DMA1_IT_TC3);
DMA_ITConfig(DMA1_Channel3, DMA_IT_TC, ENABLE);
NVIC_Struct.NVIC_IRQChannel = DMA1_Channel2_3_IRQn;
NVIC_Struct.NVIC_IRQChannelPriority = 1;
NVIC_Struct.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_Struct);
DMA_Cmd(DMA1_Channel3, DISABLE);
//Re-initialize channel
DMA_Init(DMA1_Channel3, &DMA_Struct);
//Enable the DMA channel
DMA_Cmd(DMA1_Channel3, ENABLE);
}
void DMA1_Channel2_3_IRQnHandler(void){
if(DMA_GetITStatus(DMA1_IT_TC3)){
DMA_ClearITPendingBit(DMA1_IT_TC3);
}
}
uint32_t i;
void delay()
{
for(i=0;i<0x00010000;i++);
}
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USARTs_Configuration();
DMA_Configuration();
while(1)
{
USART_SendData(USART1,'*');
delay();
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-16 8:11 AM
Does the DMA controller permit this type of peripheral-to-peripheral interaction?
Does the IRQ Handler get called? You don't need to have unique initialization structures for each pin, usart, etc. It's a throw away structure that's used once and discarded.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-17 5:20 AM
Thanks clive for your answer,is there any example Usart to Peripheral or similar application
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-17 10:15 AM
The problem with peripheral to peripheral DMA is there is no channel/stream combination to support it. That means the either the source or destination can't perform a DMA request. Then there's the bus matrix, only one AHB to APB bridge.
Yes the peripheral looks like a memory address but internally it isn't the same. The data has to be routed to different places and there has to handshake signals for the DMA to start transfers. And there's no way the DMA FIFO will work since only of the DMA handshakes (the stream) to either write to or read from the FIFO is missing. Jack Peacock- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-11-17 10:34 AM
is there any example Usart to Peripheral or similar application
Not that I've written, I'm not using Cortex-M0 parts, so no business driver there. What I do is practice and experiment based on a review of the available documentation.Up vote any posts that you find helpful, it shows what's working..