STM32C011 unbale to configure nRST pin as GPIO
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-23 1:10 AM - edited ‎2024-02-23 1:10 AM
Hi everyone,
Recently started working on STM32C011J4M3 micro. I'm trying to set PF2-NRST pin as a GPIO. but when I configure it from cube MX as GPIO PIN always reamins in High state that is a 3.28v and i'm unable to toggle the pin or perform any other operation.
int main(void)
{
/* USER CODE BEGIN 1 */
// SET_BIT(FLASH->OPTR,FLASH_OPTR_NRST_MODE_1);
WRITE_REG(FLASH->OPTR,0x2UL << 027U); // Even tried stting nrst mode2.
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_Delay(3000);
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_2, GPIO_PIN_SET);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
can anyone help me with this,
do I need to add any push-up/pull down specifically to this pin to use as GPIO?
Solved! Go to Solution.
- Labels:
-
STM32C0 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-29 3:48 AM
To configure PF2 as a GPIO (input, output, AF, or analog I/O), set the NOT_RESET_INPUT_ONLY bit and clear the NOT_GPIO_MODE_ONLY bit of the FLASH option bytes. The new setting only takes effect upon the option byte loading (OBL) event following a reset. Until the reset release, PF2 keeps acting as reset I/O. When PF2 acts as a GPIO, reset can only be triggered from one of the device internal reset sources and the reset signal cannot be output.
please see chapter 3.4.2, pages 57-58, from the STM32C0x1 advanced Arm<Sup>®</Sup>-based 32-bit MCUs - Reference manual
please make sure it is not entering continuously in the portion of the code that triggers the option byte programming, as it can only withstand around 10K cycles and this can be achieved pretty fast if left unchecked:
int main(void)
{
/* USER CODE BEGIN 1 */
FLASH_OBProgramInitTypeDef OptionsBytesStruct;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* Configure the system clock to 48 MHz */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
//Check to see if the option byte is already properly configured and only updates it if needed
HAL_FLASHEx_OBGetConfig(&OptionsBytesStruct);
if((OptionsBytesStruct.USERConfig & OB_USER_NRST_MODE )!= OB_RESET_MODE_GPIO)
{
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Unlock the Option Byte *************/
HAL_FLASH_OB_Unlock();
OptionsBytesStruct.OptionType = OPTIONBYTE_USER ; //Configure USER type
OptionsBytesStruct.USERType = OB_USER_NRST_MODE;
OptionsBytesStruct.USERConfig = OB_RESET_MODE_GPIO;//Set the NRST pin to behave only as GPIO
HAL_FLASHEx_OBProgram(&OptionsBytesStruct);
//Option byte update sequence
SET_BIT(FLASH->CR, FLASH_CR_OPTSTRT);
while((FLASH->SR & FLASH_SR_BSY1) != 0)
{
NVIC_SystemReset();//MCU will reset to perform the option byte update
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-23 2:14 AM - edited ‎2024-02-23 2:20 AM
There was an error in the definition of ports in the HAL. I don't know if it's already fixed, I reported it here.
P.S. In your code is only one dellay.
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_2, GPIO_PIN_RESET);
HAL_Delay(3000);
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_2, GPIO_PIN_SET);
HAL_Delay(3000); /* new delay */
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-23 2:42 AM
hi @ONadr.1 thanks for your response. I did check. issue is still not fixed according to your post. but this does not help me. those configurations are used for exti mode configuration and it should not be a issue for normal GPIO operation. still debigging further, will try with LL drivers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-23 2:57 AM
That problem is related to the NRST pin used as GPIO. The problem is that the base for port F, which is used as an output for the NRST pin, is incorrectly defined in the HAL code.
See the last line of base addres definition.
// original code
#define GPIO_GET_INDEX(__GPIOx__) (((__GPIOx__) == (GPIOA))? 0uL :\
((__GPIOx__) == (GPIOB))? 1uL :\
((__GPIOx__) == (GPIOC))? 2uL :\
((__GPIOx__) == (GPIOF))? 3uL : 4uL)
//new code
#define GPIO_GET_INDEX(__GPIOx__) (((__GPIOx__) == (GPIOA))? 0uL :\
((__GPIOx__) == (GPIOB))? 1uL :\
((__GPIOx__) == (GPIOC))? 2uL :\
((__GPIOx__) == (GPIOF))? 5uL : 6uL)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-29 3:48 AM
To configure PF2 as a GPIO (input, output, AF, or analog I/O), set the NOT_RESET_INPUT_ONLY bit and clear the NOT_GPIO_MODE_ONLY bit of the FLASH option bytes. The new setting only takes effect upon the option byte loading (OBL) event following a reset. Until the reset release, PF2 keeps acting as reset I/O. When PF2 acts as a GPIO, reset can only be triggered from one of the device internal reset sources and the reset signal cannot be output.
please see chapter 3.4.2, pages 57-58, from the STM32C0x1 advanced Arm<Sup>®</Sup>-based 32-bit MCUs - Reference manual
please make sure it is not entering continuously in the portion of the code that triggers the option byte programming, as it can only withstand around 10K cycles and this can be achieved pretty fast if left unchecked:
int main(void)
{
/* USER CODE BEGIN 1 */
FLASH_OBProgramInitTypeDef OptionsBytesStruct;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* Configure the system clock to 48 MHz */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
//Check to see if the option byte is already properly configured and only updates it if needed
HAL_FLASHEx_OBGetConfig(&OptionsBytesStruct);
if((OptionsBytesStruct.USERConfig & OB_USER_NRST_MODE )!= OB_RESET_MODE_GPIO)
{
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Unlock the Option Byte *************/
HAL_FLASH_OB_Unlock();
OptionsBytesStruct.OptionType = OPTIONBYTE_USER ; //Configure USER type
OptionsBytesStruct.USERType = OB_USER_NRST_MODE;
OptionsBytesStruct.USERConfig = OB_RESET_MODE_GPIO;//Set the NRST pin to behave only as GPIO
HAL_FLASHEx_OBProgram(&OptionsBytesStruct);
//Option byte update sequence
SET_BIT(FLASH->CR, FLASH_CR_OPTSTRT);
while((FLASH->SR & FLASH_SR_BSY1) != 0)
{
NVIC_SystemReset();//MCU will reset to perform the option byte update
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-16 1:26 PM
Hi everyone,
Recently started working on STM32C011J4M3. I'm trying to set PF2-NRST pin as a GPIO and I want Pin 4 to multiplexed to PA0 USART TX pin . At first i tried multiplexed the Pin 4 to PA0 using the following API " LL_SYSCFG_ConfigPinMux(LL_PINMUX_SO8_PIN4_PA0);" but this didn't work and to mention that this API function worked on Pin 1 and Pin 5 . I came across this post to set PF2-NRST pin as a GPIO and change the Pin 4 to PA0 thinking that multiplex is only done with GPIO Ports . I tried above code to set the NOT_RESET_INPUT_ONLY bit and clear the NOT_GPIO_MODE_ONLY bit of the FLASH option bytes this works in Registers but to my surprise the Pin 4 still works as PF2-NRST pin and not as GPIO . Debugging works as always and when i remove the Pin4 connection from debugger I receive console message as "Target is not responding, retrying..." I conclude that this massage show that still the Pin 4 is set as PF2-NRST pin even though the NOT_GPIO_MODE_ONLY bit is cleared . I'm really confused plz check the attachment and help me out .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-16 10:27 PM
you have to be very careful when working with this piece of code. it is mostly possible that you got locked out of your micro without setting the GPIO configuration properly.
you have to run this code first thing while running main, and once you do OB write you have to reset controller. but before flashing this code to controller you have to make sure that you have configured this pin as A gpio port pA0 in gpio init function. as you loose your access to nrst and if your SWD and SWclck is also occupied you get locked out of the system.
as far as I can see you have not configured pin as PA0 gpio in output and now you are locked out of your system.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-16 11:40 PM
Thanks for your response @pratik0199 I have Configured pin 4 as pA0 USART TX pin and this is done In USART Init function . Are you saying that I have initialize UART function to set Pin 4 to pA0 USART tx pin before calling OB write function.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-23 1:36 AM
Hello Guy,
the problem was with me i miss understood the SW1 pin of STM32C0116DK as reset pin . The code provide by @pratik0199 works great . just config PF2 as GPIO pin and using API "LL_SYSCFG_ConfigPinMux" is enough to multiples Pin4 (PF2) to PA0 .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-11 5:14 AM
There is a safer way to set the NRST pin as GPIO.
- Open STM32CubeProgrammer and connect to your target device.
- Look for the Option Bytes menu (third tab on the left).
- Unpack User Configuration menu.
- Find NRST_MODE and set it to 2 (GPIO: standard GPIO pad functionality, only internal reset possible).
- Click Apply and power cycle (or disconnect from target)