Skip to main content
shides2
Associate II
February 13, 2016
Question

STM32 QuadSPI only BANK2

  • February 13, 2016
  • 2 replies
  • 1045 views
Posted on February 13, 2016 at 11:22

Hello!I have the follow problem:I use

STM32F745. I've chosen the

QuadSPI interface for flash, to be exact,

QSPI BANK2

. I make initialization through

CUBEMX, using HAL library. I see CLK signal only, there are no other signals. I've revised the generated code of initialization - it's ok. If I initialize

QSPI BANK1 - it's ok, there are all signals. I haven't met the definite prohibition of using

BANK2 separately.

CUBE lets initializing

BANK2 without using

BANK1. Now I'm working with

BANK2 due to initializing of regime of work with 2 flashes, and signals are duplicating.

The question is: is it possible to use

BANK2 separately? Where's the bug?

Any help appreciated!

#stm32f7-quadspi-bank2
This topic has been closed for replies.

2 replies

Travis Travelstead
Associate
February 8, 2019

Did this ever get resolved? I am also curious about using just Bank2.

lliuq.1
Visitor II
April 12, 2020

hi, do you have solution now? thanks