Associate II
February 4, 2018
Question
STM32-MAT-TARGET Can not find which APB timer TIM1 is connected to.
- February 4, 2018
- 10 replies
- 5911 views
Posted on February 04, 2018 at 11:08
Hi, I've been following the manual STM32-MAT/TARGET Hands On Rev 2.2 (see attached) and I am not able to get the timer 1 working (everything is working except this). I did everything like in the manual but when I load the .ioc file into simulink I get the next error:
♯♯♯ TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 is used.
I am using the STM32F767ZI nucleo.
Anybody knows how to solve this issue? Am I missing something?
Thanks in advance!