Skip to main content
David Koss
Visitor II
April 3, 2017
Question

STM32 How to set/use the Real Time Clock

  • April 3, 2017
  • 1 reply
  • 966 views
Posted on April 03, 2017 at 17:15

Hello,

I am having issues with the Real Time clock. Occasionally it will miss its interrupt ( always when I stop the debugger )

I am not setting the date/time as I just want to have interrupt trigger a second from the current time

I have a catch so when I increment the seconds in the TR counter and it reaches 60 to set to zero so just want to make sure my code is correct

My code

      uint32_t value = 0U;

   

    // Disable the write protection for RTC registers

    RTC->WPR = 0xCAU;  

    RTC->WPR = 0x53U;

    // Disable the Alarm timer

    RTC->CR &= ~(RTC_CR_ALRAE);

 

    // Clear flag Wake-Up

    RTC->ISR &= ~( RTC_ISR_ALRAF );

  

    while((RTC->ISR & RTC_ISR_ALRAWF) != RTC_ISR_ALRAWF) /* (3) */

    {

    /* add time out here for a robust application */

    }

   

    RTC->ISR |= RTC_ISR_INIT;

    while((RTC->ISR & RTC_ISR_INITF) != RTC_ISR_INITF) /* (3) */

    {

    /* add time out here for a robust application */

    }

   

    value  = ( RTC->TR ) ;

    value = RTCBcdToByteSeconds(value); 

    value = value + 1;

    value = RTCByteToBcdSeconds( value );

    // Configure the AlarmA

    //RTC->ALRMAR = RTC_ALRMAR_MSK4 | RTC_ALRMAR_MSK3 | RTC_ALRMAR_MSK2 | RTC_ALRMAR_MSK1;

    RTC->ALRMAR = RTC_ALRMAR_MSK4 | RTC_ALRMAR_MSK3 | RTC_ALRMAR_MSK2 | value;

    //RTC->ALRMASSR = RTC_ALRMBSSR_MASKSS | ( RTC->SSR & RTC_ALRMASSR_SS );

    // Configure the Interrupt in the RTC_CR register

    RTC->CR |= RTC_CR_ALRAIE;

 

    // Enable the Wakeup Timer

    RTC->CR |= RTC_CR_ALRAE;

    RTC->ISR &= ~(RTC_ISR_INIT);

   

    // Enable the write protection for RTC registers

    RTC->WPR = 0xFFU;
    This topic has been closed for replies.

    1 reply

    Nesrine M_O
    Associate
    April 3, 2017
    Posted on April 03, 2017 at 17:32

    Hi

    koss.david

    ,

    please refer to ready example under the

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries/stsw-stm32html

    STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\STM32F4xx_DSP_StdPeriph_Lib_V1.7.0\Project\STM32F4xx_StdPeriph_Examples\RTC

    -Nesrine-