Skip to main content
Associate
August 26, 2024
Solved

ST-Link driver issue

  • August 26, 2024
  • 4 replies
  • 1310 views

Hi All,

I would need the link to download the ST-Link driver 2.1.0.0 from 08/06/2017.

The latest one is interrupting the connection to board randomly every couple of seconds.

I cannot find any link to the former ST-Link drivers, so please provide me the aforementioned one.

Thanks.

This topic has been closed for replies.
Best answer by Sebdee

Hi All,

I have solved the problem. The issue was coming from an old USB extension cable I had to connect the USB HUB to it. I have replaced this 50cm extension cable with a newer one and now it works with the latest driver.

What is still strange, is that when I connect the board directly to another single USB port on my computer, either USB 3.X or 2.X, with a new cable, this does not work. I must pass through a HUB to make it work.

Thanks

4 replies

Peter BENSCH
ST Technical Moderator
August 26, 2024

Welcome @Sebdee, to the community!

version 2.1.0.0 is very old and no longer up-to-date. There are some websites that deal with Bluepill and similar things and juggle with such old drivers, but this cannot be a clean solution.

Which board with which STM32 shows the behaviour with the interruptions in connection with which software?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SebdeeAuthor
Associate
August 26, 2024

Hi @Peter BENSCH ,

Thanks. I am using an STM32 Nucleo-F767 ZI. Up to last week everything was fine.

However, now when I connect the board to the USB port, the LD4 stays green (instead of red), and the board resets randomly and the LD4 is blinking, like when you program the board. I guess this is linked to the ST-Link. Also, when I am in STM32CubeProgrammer, the board can connect, but randomly it lost the connection with the message "Connection to device 0x451 is lost".

When I plug the same board to another computer, the LD4 is red and not green and it works perfectly without any issue. The only difference I could find between both computers was the ST-Link driver versions between them. The machine with version 2.1.0.0 works smoothly.

Thanks

SebdeeAuthor
Associate
September 20, 2024

Hi All,

I have tried with the driver version 2.1, but it still fails...

Does anyone would know why it does not work on one of my computer?

I am sur it has to do with the USB ports, that perhaps cannot maintain enough power.

I have tried with all types of USB ports (2.x, 3.x), but the behavior is always the same.

SebdeeAuthorBest answer
Associate
October 18, 2024

Hi All,

I have solved the problem. The issue was coming from an old USB extension cable I had to connect the USB HUB to it. I have replaced this 50cm extension cable with a newer one and now it works with the latest driver.

What is still strange, is that when I connect the board directly to another single USB port on my computer, either USB 3.X or 2.X, with a new cable, this does not work. I must pass through a HUB to make it work.

Thanks