Skip to main content
Mauro1
Associate
February 23, 2021
Question

Simulink Coder Support Package for P-NUCLEO-WB55 board and model-based design examples for STM32WB55

  • February 23, 2021
  • 0 replies
  • 599 views

Hello,

I have the following questions about available support in Simulink:

1) Is it planned to add Nucleo-WB55 to the set of supported boards in Simulink Coder (for example to communicate with hardware in Normal Mode Simulation using Connected IO)? If so, when will it be available?

2) Where can I find, if available, Simulink model examples for P-NUCLEO-WB55 to be used in Simulink External Mode o for STM32WB55 MCU code generation through Simulink Embedded Coder?

3) Is it planned to make available a Simulink library which includes encrypted radio stack binaries and support for modeling BLE and Thread applications? If not, are there other ways to model applications like this in Matlab/Simulink?

Thanks a lot.

Mauro 

    This topic has been closed for replies.