cancel
Showing results for 
Search instead for 
Did you mean: 

Simple integer conversion error

puneethj
Associate II
Posted on November 13, 2015 at 11:01

Hi guys i am struggling to convert 2 8bit values into 16bit value, please help me

//Global variable
volatile uint8_t data[16];
volatile uint16_t BIG;
main()
{
data[1] = 23;//msb
data[0] = 21; //lsb
BIG = data[0] | (data[1] << 8);
while(1);
}
but in the output i only get lsb.. MSB is not showing up

#stm32-c
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
AvaTar
Lead
Posted on November 13, 2015 at 11:12

>(data[1] << 8)

If the data type of

data[]

is only 8 bits in size, what do you think is left if you shift it by 8 bit ?

BIG = data[0] | ((uint16_t)data[1] << 8);

should work.
puneethj
Associate II
Posted on November 13, 2015 at 12:11

hey Avatar thanks for your time, this is 32 bit MCU the 8 bit data is moved to 32bit general purpose registers R1 or R2 before shifting so there is enough space i guess. Anyway i got the solution is some way BIG = (data[2] << 8 | data[3]);

it works thanks people

AvaTar
Lead
Posted on November 13, 2015 at 13:07

> ... this is 32 bit MCU  ...

 

You are wrong here, in the sense that this does not matter.

The behavior you are observed is defined in the C language standard. I would suggest to again read and digest especially the part about automatic type promotions.

qwer.asdf
Senior
Posted on November 13, 2015 at 16:30

@AvaTar

Sorry to say, but it's you who is wrong. The value will be implicitly converted to ''unsigned int'' (which is 32-bit on STM32) before shifting. See here for

https://stackoverflow.com/questions/18370197/does-bit-shift-automatically-promote-chars-to-int

. @jagadeesh.puneeth This code is working for me, and printing 0x1234:

int
main() {
volatile
uint8_t data[2];
volatile
uint16_t BIG;
data[0] = 0x12; 
//msb 
data[1] = 0x34; 
//lsb
BIG = data[1] | (data[0] << 8);
printf
(
''BIG = 0x%x
''
, BIG);
while
(1) {
}
}

Also, when constructing integers bigger than one byte be careful not to get the bytes in the wrong order as STM32 is

https://en.wikipedia.org/wiki/Endianness

.
puneethj
Associate II
Posted on November 13, 2015 at 21:57

Nice :) thanks man i appreciate it.