Skip to main content
Associate II
March 25, 2025
Solved

Sending UDP on NetXDuo does not work without breakpoints.

Hi, I have created a program to send UDP using NetXDuo on a Nucleo-H755ZI.
I used the URL below as a reference.

Creating a dual IPv6 & IPv4 NetXDuo UDP application for STM32H7 using CubeMX

 

I checked the operation in debug mode and could see that it is sending UDP with Wireshark.

However, when I unchecked “Set breakpoint at:main” in the debug properties and checked without breakpoints, no UDP was sent.

The version of STM32CudeIDE is 1.18.0, X-CUBE-AZRTOS-H7 version is 3.3.0.

How can I send UDP in debug mode without breakpoints or send UDP in RUN mode?

If anyone has a solution, please let me know.

 

STM32H755ZITX_FLASH.ld could not be uploaded, but the following memory is allocated.

 .tcp_sec (NOLOAD) : 
 {
 . = ABSOLUTE(0x24030000);
 *(.RxDecripSection)

 . = ABSOLUTE(0x24030080);
 *(.TxDecripSection)
 
 . = ABSOLUTE(0x24030200);
 *(.NetXPoolSection)
	
 } >RAM_D1 AT> FLASH

 

This topic has been closed for replies.
Hey0256Best answer
Associate II
March 26, 2025

Dear Neil.
Thank you for your reply.


I was surprised to see that the problem is not only a NetDuo problem, but also happens with LWIP.
I also tried updating the Ethernet status with nx_ip_interface_status_check and nx_ip_driver_direct_command, but it did not work.
In the end, adding HAL_Delay(2000) before MX_ThreadXInit() in main.c was a sure thing.
Thanks to your advice, I am now able to send UDP without any problems.
I hope this note of mine will help others.
Thank you again.

5 replies

Andrew Neil
Super User
March 25, 2025

@Hey0256 wrote:

when I unchecked “Set breakpoint at:main” in the debug properties and checked without breakpoints, no UDP was sent.


Sounds like there's something you need to wait for at the start of main...

 

https://community.st.com/t5/stm32-mcus-embedded-software/stm32f767-lwip-tcp-client/m-p/777886

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Hey0256AuthorBest answer
Associate II
March 26, 2025

Dear Neil.
Thank you for your reply.


I was surprised to see that the problem is not only a NetDuo problem, but also happens with LWIP.
I also tried updating the Ethernet status with nx_ip_interface_status_check and nx_ip_driver_direct_command, but it did not work.
In the end, adding HAL_Delay(2000) before MX_ThreadXInit() in main.c was a sure thing.
Thanks to your advice, I am now able to send UDP without any problems.
I hope this note of mine will help others.
Thank you again.

Andrew Neil
Super User
March 26, 2025

@Hey0256 wrote:

I was surprised to see that the problem is not only a NetDuo problem, but also happens with LWIP..


Which certainly suggests that the "problem" is just that something (presumably hardware?)  takes a while to "stabilise" - and you just have to wait for that to complete.

 

What this really needs is someone to look into it and find what, exactly, that thing is - and, thus, how to check for "ready" without just resorting to arbitrary, blind delays.

@ASEHST  ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Employee
June 17, 2025

Hello,

This recurring issue has been tracked internally.

An internal ticket (212424) has already been raised for follow-up.

 

With Regards.

"If your question is answered, please close this topic by clicking ""Accept as Solution""."
ST Employee
July 7, 2025

Hello,

During the initialization process, the ETH MAC must be configured with the correct Ethernet link speed and duplex mode after the auto-negotiation process is completed, which can take up to a few seconds (see the API HAL_ETH_SetMACConfig).

To resolve the issue, please add the task App_Link_Thread_Entry to your app_netxduo.c file (refer to Nx_TCP_Echo_Client example from X-CUBE-AZRTOS-H7 v3.3.0) .

This task continuously polls the PHY status and updates the MAC configuration if any changes occur to the Ethernet link.

Note: There is no need to add an additional HAL_delay().

Regards