Skip to main content
Singh.Harjit
Senior
October 21, 2020
Question

RM0440, Rev 4, STM32G4 Reference Manual - Section 27.3.9 - Error in description or Table 224

  • October 21, 2020
  • 1 reply
  • 497 views

On page 894 the paragraph just above Table 224 says:

Table 224 gives

the 8 available options per timer: CMPx refers to blanking from counter reset to compare

match, Tx2 refers to the timing unit TIMx output 2 waveform defined with HRTIM_SETx2

and HRTIM_RSTx2 registers. For instance, timer B (TIMFLTR6) is timer C output 2

waveform.

If you look at the Destination, Timer B row, there is a "-" under timer C output 2 (TD2) column.

Timer C output 2 (TD2) appears to connect to Timer D (TIMFLTR6).

Timer B (TIMFLTR6) is Timer F CMP2.

Is the text above the table incorrect or is Table 224 incorrect?

Thank you.

This topic has been closed for replies.

1 reply

Imen GH
ST Employee
October 23, 2020

Hello,

The table is correct.

I raised internally  your feedback to correct the error in next release.

Thank you.

Imen