Skip to main content
Associate III
May 11, 2024 4:30 PM UTC
Solved

Register bits missing in STM32CubeProgrammer

I stumbled across this problem:

https://community.st.com/t5/stm32-mcus-products/unable-to-read-reset-values-of-the-stm32h730vb-octospim/m-p/212094

In the current rev 3 of RM0468 https://www.st.com/resource/en/reference_manual/rm0468-stm32h723733-stm32h725735-and-stm32h730-value-line-advanced-armbased-32bit-mcus-stmicroelectronics.pdf I see this register bit:

pkoevesdi_2-1715444936114.png

But the same register looks quite different in the STM32CubeProgrammer:

pkoevesdi_1-1715444512232.png

 

Also, there's a typo in the table on Bit 19, must say OCTOSPI2EN

 

Am I doing/expecting something wrong, or ist it a bug. If second, is someone reading here who can address it at STM?

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
May 13, 2024 8:37 AM UTC

Hello @pkoevesdi ,

Thank you for bringing this issue to our attention.

I reported this issue internally.

To solve the wrong register bits description, could you please try to download the SVD file from this link  .

Unzip the file, then copy STM32H73x.svd file and paste it into the STM32Cubeprogrammer installation folder "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\SVD".

I hope this help you.

Internal ticket number: 181193 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
May 13, 2024 8:37 AM UTC

Hello @pkoevesdi ,

Thank you for bringing this issue to our attention.

I reported this issue internally.

To solve the wrong register bits description, could you please try to download the SVD file from this link  .

Unzip the file, then copy STM32H73x.svd file and paste it into the STM32Cubeprogrammer installation folder "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\SVD".

I hope this help you.

Internal ticket number: 181193 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
pkoevesdiAuthor
Associate III
May 13, 2024 4:38 PM UTC

Thank You, with this file, at least the mentioned register conforms to the RM.