Skip to main content
Associate II
January 14, 2025
Solved

Read uninitialized SRAM values

  • January 14, 2025
  • 4 replies
  • 1172 views

Hello and thanks in advance for reading my post.

 

I am currently working on my dissertation, trying to implement a digital signing algorithm on a Arm Cortex-M0+ microprocessor. I'm using a NUCLEO-G0B1RE board with a stm32 with the same series. This board does not come with a TRNG peripheral and I don't want to use a packaged one, as I'm trying to understand the process of crceating an RNG as well.

From some posts I have read (either on this forum or other ones), it seems that uninitialized SRAM is a good starting point for my entropy source. I'm also taking into consideration using time jitter between two oscillators (mainly the 32 kHz +- 5% RC oscillator and the PLL block).

I use VSCode and I wrote my own linker script and startup code.

I have created a noinit section that loads into SRAM:

 .noinit (NOLOAD) : {
 *(.noinit)
 } >SRAM

SRAM is a memory zone which has the origin and length based on the memory organization chapter in the reference manual and is according to my device specifications:

 SRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 144K

I have also created a volatile array of unsigned integers to be loaded in the noinit section:

volatile uint8_t au8Arr[1024] __attribute__((section(".noinit")));

When using Cortex-Debugger to check the values inside au8Arr in the Reset_Handler, there seems to be very little if any modification at all in bytes.

It seems that SRAM is retained even on longer power cycles (1min - 10min).

 

My question is how can I make the retention period much smaller (if none at all) or how can I adapt to these behaviour?

This topic has been closed for replies.
Best answer by Andrew Neil

As it says in your 1st link, the randomness is "biased" by process variations - I don't think it's safe to assume that "bias" won't completely swamp other random effects?

 


@undacmic wrote:
  • Temperature sensor LSB? (it just seems that it is susceptible to external alterations of temperature that might result in pretty stable ADC reads)

That's why you consider only the LSB - that's always going to be the least stable.

 


@undacmic wrote:
  • Time jitter?

Yes, that's a common one

 


@undacmic wrote:
  • What can I do to read the analogue values within the memory array?

Nothing - that's hidden by the hardware.

 


@undacmic wrote:
  • Any other way?

Yes, many - what's practical/useful depends on the specific application.

If there were just one, simple, universal way - then chipmakers wouldn't have to go to lengths to provide TRNGs!

4 replies

Andrew Neil
Super User
January 14, 2025

@undacmic wrote:

From some posts I have read (either on this forum or other ones), it seems that uninitialized SRAM is a good starting point for my entropy source


I don't think so - perhaps you are misinterpreting those posts?

While there are some proposals that do use uninitialised memory, I think they look at the analogue values within the memory array?

What you read via software is quantised into just '1' or 'zero' - so you lose the vast majority of the entropy.

The digital values that code reads from uninitialised memory do tend to be pretty constant.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
undacmicAuthor
Associate II
January 14, 2025

Honestly, it is my first time doing an embedded project and I might be misguided, but here is a list of what I've found, again I am not saying this is a correct implementation, is just that some other people seem to have tried, and using NIST statistical tests to prove the usability of the entropy source seemed good for me:

Ok, now let's say this is an incorrect assumption, what approach I should take for using only the board for entropy?

  • Temperature sensor LSB? (it just seems that it is susceptible to external alterations of temperature that might result in pretty stable ADC reads)
  • Time jitter?
  • What can I do to read the analogue values within the memory array?
  • Any other way?

 

Andrew Neil
Andrew NeilBest answer
Super User
January 14, 2025

As it says in your 1st link, the randomness is "biased" by process variations - I don't think it's safe to assume that "bias" won't completely swamp other random effects?

 


@undacmic wrote:
  • Temperature sensor LSB? (it just seems that it is susceptible to external alterations of temperature that might result in pretty stable ADC reads)

That's why you consider only the LSB - that's always going to be the least stable.

 


@undacmic wrote:
  • Time jitter?

Yes, that's a common one

 


@undacmic wrote:
  • What can I do to read the analogue values within the memory array?

Nothing - that's hidden by the hardware.

 


@undacmic wrote:
  • Any other way?

Yes, many - what's practical/useful depends on the specific application.

If there were just one, simple, universal way - then chipmakers wouldn't have to go to lengths to provide TRNGs!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.