Question about SPI2 using PC_2 and PC_3
My project (Stm32H753) has 2 identical external ADCs, one on SPI2 and one on SPI3. The one on SPI3 is working fine, but I am having problems with SPI2. The code for them are the same, except of course different 'hspi' and pin assignments.
The SPI is configured to use PC2 and 3 as MISO and MOSI, I probed SPI signals, everything looked fine except on MISO (ADC output) the voltage is only 1Vpp. Open the analog switches (SYSCFG->PMCR) didn't help much (instead reading all 0s, openning the switches gives all 0xfff readings. I have internal pullup for MISO).
Just curious, when PC_2 and PC_3 are labeled with '_', are there any special steps to use them for SPI2?