PWM output example for Stm32f4 is so confusing
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-07-11 12:25 AM
Hi, I trried to understand how to calculate pwm output from example that comes with Stm32f4-Discovery-FW1.1.0. The file is in Project > Peripheral_Examples > TIM_PWM_Output > main.c
This is the most confusing part in comment/* -----------------------------------------------------------------------
TIM3 Configuration: generate 4 PWM signals with 4 different duty cycles.
In this example TIM3 input clock (TIM3CLK) is set to 2 * APB1 clock (PCLK1),
since APB1 prescaler is different from 1.
TIM3CLK = 2 * PCLK1
PCLK1 = HCLK / 4
=> TIM3CLK = HCLK / 2 = SystemCoreClock /2
To get TIM3 counter clock at 28 MHz, the prescaler is computed as follows:
Prescaler = (TIM3CLK / TIM3 counter clock) - 1
Prescaler = ((SystemCoreClock /2) /28 MHz) - 1
To get TIM3 output clock at 30 KHz, the period (ARR)) is computed as follows:
ARR = (TIM3 counter clock / TIM3 output clock) - 1
= 665
TIM3 Channel1 duty cycle = (TIM3_CCR1/ TIM3_ARR)* 100 = 50%
TIM3 Channel2 duty cycle = (TIM3_CCR2/ TIM3_ARR)* 100 = 37.5%
TIM3 Channel3 duty cycle = (TIM3_CCR3/ TIM3_ARR)* 100 = 25%
TIM3 Channel4 duty cycle = (TIM3_CCR4/ TIM3_ARR)* 100 = 12.5%
Note:
SystemCoreClock variable holds HCLK frequency and is defined in system_stm32f4xx.c file.
Each time the core clock (HCLK) changes, user had to call SystemCoreClockUpdate()
function to update SystemCoreClock variable value. Otherwise, any configuration
based on this variable will be incorrect.
----------------------------------------------------------------------- */
My problem are; 1) System Clock is 168 MHz and If I need to get 28Mhz, my prescaler should be 6 - 1. Isn't it? From this comment, prescaler is set to 3 - 1.2) To calculate ARR value, we need to use this equation; ARR = (TIM3 counter clock / TIM3 output clock) - 1Where ''TIM3 counter clock'' is 28 MHzand ''TIM3 output clock'' is 30 Khz so we get ARR = (28MHz / 30 KHz) -1 = 933 - 1 = 932why they get ARR = 655... ??????????? where is this magic number come from?Thanks for your help #stm32f4-pwm-output-example- Labels:
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-07-11 1:57 AM
TIM3CLK = HCLK / 2 =
SystemCoreClock / 2
so TIM3 is clocked at 84MHz. Consequently the prescaler value (3-1) is correct for 28MHz. (Take a look at the device overview and clock tree diagrams to work out what's going on. Note that APBx prescaler has an odd operation where frequencies are doubled if prescaler is not 1.) However, the example in the STM32F4 STM32F4xx_DSP_StdPeriph_Lib_V1.0.1 uses a 21MHz clock. For a 21MHz clock the ARR value of 665 does result in about a 30kHz rate. 21MHz / 666 = 31.531...kHz. I think someone just copied the code without thinking!- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-07-11 4:13 AM
Thanks for clarify
moodaeng