Skip to main content
DMala.1
Associate II
April 10, 2020
Question

Problem with STM32L475 Discovery kit IoT node power supply

  • April 10, 2020
  • 4 replies
  • 1253 views

Hello, I've just received the STM32L475 Discovery kit IoT node. I connected the board through USB cable to my laptop (the JP4 jumper is connected to 5V_ST_LINK) and the power supply LED (LD5) is blinking. Also the board is not visible from laptop (I have installed the required drivers). What is going on? Is there something else I have to do?

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
April 11, 2020

Make sure not to use a charging cable, these only have power lines, and lack the data lines for connectivity.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DMala.1
DMala.1Author
Associate II
April 11, 2020

Hi, thank you for your answer. The problem seems to be the power supply, that's why the board is not visible. The power supply LED should be on and not blinking. ​

Pavel A.
April 11, 2020

> Also the board is not visible from laptop (I have installed the required drivers).

Are you sure? Have you looked in Devices and Printers, or used a tool such as USBview?

-- pa

DMala.1
DMala.1Author
Associate II
April 11, 2020

Hi, thank you for your answer. The problem seems to be the power supply, that's why the board is not visible. The power supply LED should be on and not blinking. ​