Skip to main content
Visitor II
June 4, 2024
Question

problem in generating hse

  • June 4, 2024
  • 1 reply
  • 639 views

we are using UFBGA 132 for BLDC motor control with HSI clock to reduce the power consumption, we have been trying out with HSE clock by enabling PD10 to high, hereby, if we try to debug it get struck in the error handler function and the status of the clock was timeout. Anyone.

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
June 5, 2024

Hello,

Need to provide more details:

- The platform you are using.

- The MCU part number.

- "if we try to debug it get struck in the error handler function and the status of the clock was timeout" -> need to provide which API is returning the error.

Thank you.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.