Skip to main content
mwylie
Associate
August 13, 2015
Question

PROBLEM: External pull-up of FT pin not reaching 5V

  • August 13, 2015
  • 1 reply
  • 595 views
Posted on August 13, 2015 at 19:10

Hi,

I am having trouble using an external pull up resistor to 5V. The voltage at the GPIOs is clamping to ~3.65V. Notes:
  • Processor: STM32L151VBT6 (100-LQFP)
  • Test Board: Proprietary (nothing else connected to these pins, not even protection diodes)
  • Pins tested: PD8 and PD9
  • MCU Supply voltage: 3.0V
  • Pull-up voltage: 5.0V
  • Pull-up Resistor: 1.5 kOhm
  • A fix not requiring a board change would be best
Test code:

int main( void )
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOD, ENABLE );
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOD, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOD, &GPIO_InitStructure);
while(1);
}

What I've done so far:
  • Tested two GPIOs PD8/PD9
  • Tried configuring the pins as inputs/outputs/AF(USART) (all worked as desired except the pull up was clamped)
  • Tried different pull ups (1.5k and 5.6k)
  • Searched the forums, couldn't find anything except that pins with analog features are clamped to 3.3V, but these pins don't have any analog functionality.

Any help would be greatly appreciated.

Thanks! #stm32 #5v #ft #pull-up
    This topic has been closed for replies.

    1 reply

    mwylie
    mwylieAuthor
    Associate
    September 10, 2015
    Posted on September 10, 2015 at 14:47

    Turns out it was a burnt MCU. I replaced it and everything works fine now.