Skip to main content
matteo239955_st
Associate III
Jan 9, 2017 7:37 AM UTC
Question

Problem Encoder on STM32F071

Posted on January 09, 2017 at 08:37

Hi,

 I'm using XCube for init a SMT32F071CBT6 with Keil V5, I need to use the encoder periphery. (ALL to the last version)

In attachment three file. The project and the 2 file modify after generation.

I've use 4 alternative pins, because the other are use by an other periphery.

When start the encoder the 2 pins become output and go Low. Why?

After this command:

  HAL_TIM_Encoder_Start(&htim3, TIM_CHANNEL_ALL);

I' ve try with tim1 with exactly the same code with no problem.

Please help me.

#encoder-stm32f0
This topic has been closed for replies.

5 replies

ST Technical Moderator
Jan 9, 2017 4:55 PM UTC
Posted on January 09, 2017 at 17:55

Dear

Bandini.Matteo

‌,

I've use 4 alternative pins ..

Which alternative pins are you using ?

Could you please provide more details about your

G

PIO configuration ?

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
matteo239955_st
Associate III
Jan 10, 2017 8:29 AM UTC
Posted on January 10, 2017 at 08:29

/* USER CODE END TIM2_MspInit 0 */

/* Peripheral clock enable */

__HAL_RCC_TIM2_CLK_ENABLE();

/**TIM2 GPIO Configuration

PA15 ------> TIM2_CH1

PB3 ------> TIM2_CH2

*/

GPIO_InitStruct.Pin = GPIO_PIN_15;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_PULLUP;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF2_TIM2;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_InitStruct.Pin = GPIO_PIN_3;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_PULLUP;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF2_TIM2;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN TIM2_MspInit 1 */

HAL_TIM_Encoder_Start(&htim2, TIM_CHANNEL_ALL);

/* USER CODE END TIM2_MspInit 1 */

/* USER CODE BEGIN TIM3_MspInit 0 */

/* USER CODE END TIM3_MspInit 0 */

/* Peripheral clock enable */

__HAL_RCC_TIM3_CLK_ENABLE();

/**TIM3 GPIO Configuration

PB4 ------> TIM3_CH1

PB5 ------> TIM3_CH2

*/

GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_PULLUP;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF1_TIM3;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN TIM3_MspInit 1 */

HAL_TIM_Encoder_Start(&htim3, TIM_CHANNEL_ALL);

/* USER CODE END TIM3_MspInit 1 */
waclawek.jan
Super User
Jan 10, 2017 8:50 AM UTC
Posted on January 10, 2017 at 08:50

And TIM2/TIM3 configuration?

Rather than code, please provide the read-back content of the TIM2/TIM3 registers at the point when the problem occurs.

matteo239955_st
Associate III
Jan 10, 2017 7:56 AM UTC
Posted on January 10, 2017 at 08:56

/* TIM2 init function */

void MX_TIM2_Init(void)

{

TIM_Encoder_InitTypeDef sConfig;

TIM_MasterConfigTypeDef sMasterConfig;

htim2.Instance = TIM2;

htim2.Init.Prescaler = 0;

htim2.Init.CounterMode = TIM_COUNTERMODE_UP;

htim2.Init.Period = 65535;

htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

sConfig.EncoderMode = TIM_ENCODERMODE_TI1;

sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;

sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;

sConfig.IC1Prescaler = TIM_ICPSC_DIV1;

sConfig.IC1Filter = 0;

sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;

sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;

sConfig.IC2Prescaler = TIM_ICPSC_DIV1;

sConfig.IC2Filter = 0;

if (HAL_TIM_Encoder_Init(&htim2, &sConfig) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

}

/* TIM3 init function */

void MX_TIM3_Init(void)

{

TIM_Encoder_InitTypeDef sConfig;

TIM_MasterConfigTypeDef sMasterConfig;

htim3.Instance = TIM3;

htim3.Init.Prescaler = 0;

htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

htim3.Init.Period = 65535;

htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

sConfig.EncoderMode = TIM_ENCODERMODE_TI1;

sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;

sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;

sConfig.IC1Prescaler = TIM_ICPSC_DIV1;

sConfig.IC1Filter = 0;

sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;

sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;

sConfig.IC2Prescaler = TIM_ICPSC_DIV1;

sConfig.IC2Filter = 0;

if (HAL_TIM_Encoder_Init(&htim3, &sConfig) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

}

Mark Shoe
Associate III
May 3, 2017 3:09 PM UTC
Posted on May 03, 2017 at 17:09

The structure TIM_Base_InitTypeDef does not have a member AutoReloadPreload. However CubeMX does generate this code. The old version of CubeMX doen not generate the autoreload line in tim.c So just comment it out every time you generate new code by CubeMX.