Question
OTA IN STM32U575 USING ESP32
IS ANY BODY HELP ME IN THE OTA OF THE STM32U575 USING THE ESP32
1. HOW TO SETUP THE SYSTEM BOOTLOADER TO RECEIVE THE FIRMWARE (.BIN FILE) VIA UART AND HOW TO SELECT WHICH UART TO USE FOR UPLOAD , THERE ARE MORE UART WHICH SUPPORT THE UART FLASHING HOW TO ACTIVATE THE DESIRED UART FOR THE FIRMWARE UPLOAD
2. PLEASE SHARE ME ANR RESOUSE REGARDING SYSTEM BOOTLOADER CONFIGURATIONS
3. PLEASE SHARE ANY ESP32 FIRMWARE TRANSMIT THE BINARY FILE VIA UART