Skip to main content
abdulsamadzahir
Visitor II
January 29, 2019
Question

Nucleo F303RE LED API from BSP unavailable in Keil uVision 5.26.2.0

  • January 29, 2019
  • 0 replies
  • 1009 views

I'm using Nucleo F303RE board and I'm trying to set it up on Keil uVision v5.26.2.0 and use the LED API, but the LED API doesn't seem to be available for this board. How can I get the LED API (without STM32CubeMx)?

Here are some additional details:

  1. In Keil Pack Installer, I can select STM32F303RE to install Keil::STM32F3xx_DFP v2.1.0. However, in Manage Run-Time Environment, I only have STM32303E-Eval and STM32F3-CubeMx - no STM32F303RE. I've tried downloading BSP from Keil as well, but no use, I'm afraid. Any way to go around this?
  2. Worst comes to worst, I can opt to use STM32CubeMx. How can I actually use STM32CubeMx? I've tried and ended up with multiple instances of STM32CubeMx without them actually doing anything.

Any advice is appreciated! Thanks

0690X000006DHcnQAG.png

0690X000006DHciQAG.png

This topic has been closed for replies.