2019-12-13 8:26 AM
The ARM-M7 supports non-aligned memory accesss using LDR and STR
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0646a/BABFAIGG.html
but it isn't working for me. I'm reading and write to/from DTCMRAM.
Is there anything I need to do to get this to work? Current MPU access set up as below
/* Configure the MPU attributes as WB-nWA for SRAM */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x24000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE ;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);Thanks
2019-12-13 9:17 AM
Is it faulting? Should work without any intervention.
LDRD, STRD will fault with unaligned addresses, these are often used by the optimizer or floating point doubles.
Stack alignment for load/store multiple and pointer reads might also be a consideration.