Skip to main content
c_pbola
Visitor II
June 6, 2013
Question

Need sample source for SRAM test

  • June 6, 2013
  • 2 replies
  • 953 views
Posted on June 06, 2013 at 10:09

We are STM32F207 processor for one of our application. We used 16MB PSRAM. Now I want to test PSRAM as part of diagnostic software.

From googling I came to know that STM provides 'self-diagnostic software modules developed by ST for the STM32 family'. 

Can some one let me know how to get above mentioned software?

Also sample software for RAM testing also useful for me.

#sample-code-for-sram-test
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    June 6, 2013
    Posted on June 06, 2013 at 13:12

    Contact your local ST rep or FAE for the self test software.

    How thoroughly do you want to test the RAM, and how long of a test can you tolerate?

    A basic test would be to do an alternating/walking bit pattern that should catch stuck-at faults, and address line issues. ie try to ensure all bits can be set high/low (data pattern, then inverse), and an address specific value that is divisible by a prime rather than a power of two.

    With a slight amount of thought you should be able to detect a significant number of failures very quickly. Things which would harder to test for are intermittent and marginal timing issues.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    frankmeyer9
    Associate III
    June 6, 2013