cancel
Showing results for 
Search instead for 
Did you mean: 

N6 peripherals compatibility to other STM32 / H7 ?

LCE
Principal II

Heyho,

just found that the N6 has gigabit ethernet - which might help me staying away from the monstrous MPUs... :D

Is there kinda compatibility list between the STM32 families for the peripherals?

  • ethernet interface, surely different HW concerning GbE vs 100M, but maybe the registers / descriptors work basically the same?
  • CANFD and the SAIs?
  • OCTOSPI / XSPI with memory-mapped HyperRam? 
  • the (partly) more simple peripherals like ADC, timers, UART?

Merci!

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Not obvious to provide an exhaustive list of peripherals compatibility between N6 and H7.

Generally speaking, new products feature either the same previous versions of the peripherals from older products, or newer versions with new features or completely new architecture features which is the case of the Eth.

For ADC, Timers, UARTs most probably they are the same, may be with a slight difference in term of triggers and connections with other DMAs. 

I think better, to speed up your findings, is to look at the first chapter "main features" in the RMs of each peripheral description and compare + do a comparison of register mapping at the end of the chapter.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Andrew Neil
Super User

More generally, it would be useful to have this across all families for all the IP blocks.

I think @waclawek.jan has brought this up before ...

 

PS:

Might be a good question to ask the new ST Sidekick AI agent ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Employee

Hello,

Not obvious to provide an exhaustive list of peripherals compatibility between N6 and H7.

Generally speaking, new products feature either the same previous versions of the peripherals from older products, or newer versions with new features or completely new architecture features which is the case of the Eth.

For ADC, Timers, UARTs most probably they are the same, may be with a slight difference in term of triggers and connections with other DMAs. 

I think better, to speed up your findings, is to look at the first chapter "main features" in the RMs of each peripheral description and compare + do a comparison of register mapping at the end of the chapter.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.