Multiplexing with STM32F303
Hello !
I really need your help , im working on a project and its a game of luck , random numbers will appear on 4 x 7 Segments , so i must multiplex , i understood the principe but i can't reach some good results , i don't know why ...
only the common segment will always be on and the others off when im trying to test something on main .
example > 1234 only the segment b will be on . i ll be sharing my code and circuits and some photos thank you for your help !
Circuit http://www.fritzler-avr.de/HP/tipps/multi.php first photo
> the 4 Bases are going ofc to ports of the Stm , segments are connected to eachothers and then to stm, Collectors the Common Anodes like in the photo
Code :
#include "stm32f3xx.h"
#include <stdint.h>
void activation();
void showdigit (int digit);
void showdigits1 (int number);
void showdigits2 (int number);
void showdigits3 (int number);
void showdigits4 (int number);
void delay(unsigned int x);
void mode1 () ;
void mode2 () ;
void mode3 () ;
void mode4 () ;
int main(void){
int x = 1234 ;
activation() ;
for(;;){
mode1() ;
showdigits1(x);
delay(1000);
mode2() ;
showdigits2(x);
delay(1000);
mode3() ;
showdigits3(x);
delay(1000);
mode4();
showdigits4(x);
delay(1000);
}
}
//Delay function
volatile _Bool finished;
void delay(unsigned int x){
finished = 0;
RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
TIM2->DIER = TIM_DIER_UIE; // Update-Interrupt
TIM2->CNT = 0; TIM2->PSC = 7999; // 1 ms
TIM2->ARR = x - 1;
TIM2->CR1 = TIM_CR1_CEN; // Timer on
NVIC_EnableIRQ(TIM2_IRQn);
while (!finished)
__WFI(); TIM2->CR1 = 0;
return;
}
void TIM2_IRQHandler(void) {
finished = 1;
TIM2->SR &= ~TIM_SR_UIF; }
// end Delay Function
// Begin digitsfrom 0
void activation(){
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; // activation PORTS A
RCC->AHBENR |= RCC_AHBENR_GPIOBEN; // activation PORTS B
RCC->AHBENR |= RCC_AHBENR_GPIOCEN; // activation PORTS C
GPIOA->MODER |= 0b01 << 0; // segment d
GPIOA->MODER |= 0b01 << 2; // segment f
GPIOA->MODER |= 0b01 << 8; // segment e
GPIOA->MODER |= 0b01 << 16 ; // segment c
GPIOB->MODER |= 0b01 << 0; // segment g
GPIOC->MODER |= 0b01 << 2; // segment a
GPIOC->MODER |= 0b01 << 0; // segment b
GPIOB->MODER |= 0b01 << 20; // transistor1
GPIOB->MODER |= 0b01 << 10; // transistor2
GPIOB->MODER |= 0b01 << 12; // transistor3
GPIOA->MODER |= 0b01 << 18 ; //transistor4
}
/* PORTS DESCIPTION
Segment a PC1
Segment b PC0
Segment c PA8
Segment d PA0
Segment e PA4
Segment f PA1
Segment g PB0 */
// 0 is active emmeter => +VCC
void digit0 (){ // 0
GPIOB->ODR |= (1<<0);
}
void digit1 (){// 1
GPIOC->ODR |= (1<<1);
GPIOA->ODR |= (1<<1);
GPIOB->ODR |= (1<<0)
GPIOA->ODR |= (1<<4);
GPIOA->ODR |= (1<<0);
}
void digit2 (){// 2
GPIOA->ODR |= (1<<8);
GPIOA->ODR |= (1<<1);
}
void digit3 (){// 3
GPIOA->ODR |= (1<<4);
GPIOA->ODR |= (1<<1);
}
void digit4 (){// 4
GPIOC->ODR |= (1<<1);
GPIOA->ODR |= (1<<4);
GPIOA->ODR |= (1<<0);
}
void digit5 (){// 5
GPIOC->ODR |= (1<<0);
GPIOA->ODR |= (1<<4);
}
void digit6 (){// 6
GPIOC->ODR |= (1<<0);
}
void digit7 (){// 7
GPIOA->ODR |= (1<<4);
GPIOB->ODR |= (1<<0);
GPIOA->ODR |= (1<<1);
GPIOA->ODR |= (1<<0);
}
void digit8 (){// 8
}
void digit9 (){// 9
GPIOA->ODR |= (1<<4);
}
void showdigit (int digit) {
switch (digit)
{
case 0: digit0 ();
break;
case 1: digit1 ();
break;
case 2: digit2 ();
break;
case 3: digit3 ();
break;
case 4: digit4 ();
break;
case 5: digit5 ();
break;
case 6: digit6 ();
break;
case 7: digit7 ();
break;
case 8: digit8 ();
break;
case 9: digit9 ();
break;
default:
break;
};
};
// end digitsdefine from 0 to 9 and showing them
void showdigits1 (int number){
int x = number / 1000 ;
showdigit(x);
}
void showdigits2 (int number){
int y = (number % 1000) / 100 ;
showdigit(y);
}
void showdigits3 (int number){
int z = (number % 100) / 10 ;
showdigit(z);
}
void showdigits4 (int number){
int e = number % 10 ;
showdigit(e);
}
void mode1 () { // transistor 1 ON others OFF
GPIOA->ODR |= (1<<9);
GPIOB->ODR |= (1<<5);
GPIOB->ODR |= (1<<6);
GPIOB->ODR ^= (1<<10);
}
void mode2 () { // transistor 2 ON others OFF
GPIOA->ODR |= (1<<9);
GPIOB->ODR |= (1<<10);
GPIOB->ODR |= (1<<6);
GPIOB->ODR ^= (1<<5);
}
void mode3 () { // transistor 3 ON others OFF
GPIOA->ODR |= (1<<9);
GPIOB->ODR |= (1<<5);
GPIOB->ODR |= (1<<10);
GPIOB->ODR ^= (1<<6);
}
void mode4 () { // transistor 4 ON others OFF
GPIOB->ODR |= (1<<10);
GPIOB->ODR |= (1<<5);
GPIOB->ODR |= (1<<6);
GPIOA->ODR ^= (1<<9);
}