Skip to main content
SARTHAK KELAPURE
Associate III
December 29, 2017
Solved

MQTT using STM32L0

  • December 29, 2017
  • 9 replies
  • 6763 views
Posted on December 29, 2017 at 13:54

Hello everyone, I am trying to use MQTT protocol on my STM32 board with SIM7000 as slave. if anyone had worked in such fashion, please can you share code snippets or library file used?? Is there any generalized library file for STM32?

Thank you

#stm32 #stm32l0 #stm32l0-stm32l0-discovery #mqtt
This topic has been closed for replies.
Best answer by Andrew Neil
Posted on December 29, 2017 at 14:45

Like other internet protocols, MQTT is entirely independent of the underlying hardware.

So just try googling something like, 'MQTT microcontroller client'

9 replies

Andrew Neil
Andrew NeilBest answer
Super User
December 29, 2017
Posted on December 29, 2017 at 14:45

Like other internet protocols, MQTT is entirely independent of the underlying hardware.

So just try googling something like, 'MQTT microcontroller client'

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
francis kumar
Associate
February 23, 2018
Posted on February 23, 2018 at 09:29

Hi,

I am also looking the same mqtt microcontroller client support in any ST series.

rgds

Andrew Neil
Super User
February 23, 2018
Posted on February 23, 2018 at 09:46

Again, it has nothing specifically to do with ST.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
February 23, 2018
Posted on February 23, 2018 at 10:07

See: 

https://community.st.com/0D70X000006SsnWSAS

 
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
sne_123
Associate III
October 7, 2020

@SARTHAK KELAPURE​ Hi , I am also trying to work on the same thing as you have mentioned. Can you guide me a little bit on this?

sne_123
Associate III
October 7, 2020

I am also using Sim808 with Stm32F103 board. So for Mqtt to work on stm32, do I need to configure TCP/IP using sim808 and then use Paho mqtt library??