Skip to main content
Associate III
October 21, 2024
Solved

Minimum external clock requirement for STM32G474CET3

Hi I am using below controller in one of our design

STM32G474CET3

 

i would like to know minimum external clock frequency on which my microcontroller works.

 

Also my requirement includes 1 SPI, 1 I2C and 4 ADC input sensing.

 

I would need very minimum external clock frequency on which it can ru,

And ultimate goal is to run 1 SPI, 1 I2C and 4 ADC input sensing at a very low current consumption for 3.3V microcontroller supply,

 

In datasheet its mentioned from 4 MHz, can this be used in 1 to 3 MHz range too

sag_0-1729494067687.png

Also any ball park current consumption can i get for 1 SPI, 1 I2C and 4 ADC input sensing at 3.3V input to Microcontroller.

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
October 21, 2024

Hello @sag 

This MCU minimum HSE resonator Frequency is 4MHz. You can't use any other value under 4MHz.

For the Current consumption of your MCU, you may can refer to the Table 35 of the DS12288. 

Ps: don't forget to read the description of the Table 35.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

11 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
October 21, 2024

Hello @sag 

This MCU minimum HSE resonator Frequency is 4MHz. You can't use any other value under 4MHz.

For the Current consumption of your MCU, you may can refer to the Table 35 of the DS12288. 

Ps: don't forget to read the description of the Table 35.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
October 21, 2024

@STTwo-32 wrote:

This MCU minimum HSE Frequency is 4 MHz. You can't use any other value under 4MHz.


But, when operating with an external clock source (so not using the HSE oscillator), there is no minimum limit stated:

AndrewNeil_2-1729499372755.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
sagAuthor
Associate III
October 23, 2024

So can i connect 1 MHz then if lower is not mentioned at clock generated from an external source.

Same for 2 MHz external clock

AScha.3
Super User
October 21, 2024

Hi,

Why not use the HSI ?

No external clock needed at all.

If you feel a post has answered your question, please click on " Best Answer ".
sagAuthor
Associate III
October 21, 2024

Our operating temperature is 180 deg C which will cause drift in internal oscillator at higher temperature.

The stability is not good at higher temperature. 

Andrew Neil
Super User
October 21, 2024

@sag wrote:

Our operating temperature is 180 deg C . 


That's well outside the specified operating limits:

AndrewNeil_0-1729499813130.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
October 21, 2024

@sag wrote:

In datasheet its mentioned from 4 MHz, can this be used in 1 to 3 MHz range too


The datasheet defines the guaranteed operating conditions - if says 4MHz is the limit, then that is the limit for guaranteed operation.

AndrewNeil_1-1729499155186.png

 

If you want a lower-speed external clock, there's LSE:

AndrewNeil_0-1729499086512.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
October 21, 2024

@sag wrote:

I would need very minimum external clock frequency ... at a very low current consumption


Note that, for low(est) power consumption, it is often better to run the microcontroller fast - so that it can sleep longer.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Uwe Bonnes
Chief
October 23, 2024

For external clock, not external crystal, there is no lower limit.