Skip to main content
AP_040
Senior
February 11, 2019
Question

Migrating Nucleo-L152RE to STM32L462CE

  • February 11, 2019
  • 4 replies
  • 804 views

I have developed my application in Nucleo-L152RE board by using Atollic Truestudio. Now, I want it to migrate to STM32L462CE MCU. So, how I do that in a quick way by using Atollic Studio? Can you provide some quick steps and settings which I have to change in Atollic studio for doing this stuff?.

This topic has been closed for replies.

4 replies

ST Technical Moderator
February 12, 2019

Hello @Community member_SLS (System Level Solution)​ ,

I recommend you to follow this application note "AN4612 Application note Migrating from STM32L1 Series to STM32L4 Series and STM32L4+ Series microcontrollers" which helps you to migrate from STM32L1 Series to STM32L4 Series.

You can take this Application Note as reference to determine differences between the two series with give attention to pinout, peripherals and system clock...

The advantage of HAL library is that functions' names are the same for all series, so the migration from one device to another is not so complicated.

You may also start from the template project in the STM32CubeL1 package and then add your own modifications (new functions, new files)...

Maybe this video (migration using Keil) helps you to understand the principle of migration: https://st-videos.s3.amazonaws.com/gettindstartedsmt32cubefinal.mp4

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
February 12, 2019

How easy this is depends on how well your code is abstracted.

I'd suggest creating a small shell project for the new target, get the clock, pins and USARTs up first, and then merge sections of code across, pulling and refactoring the peripheral support as you go.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AP_040
AP_040Author
Senior
February 13, 2019

Thanks for your valuable help. I have successfully migrate my application from STM32L1 to STM32L4.

AP_040
AP_040Author
Senior
February 13, 2019

Hello @Imen DAHMEN​ ,

Thanks for you help..!!!

I have migrate my application all modules has worked fine except flash and there is one issue on writing the data into STM32L462CE flash memory.

I have checked and found that if we want to store data into flash memory, we have to store in 8 byte(double word) so, here my requirement is to store data byte by byte which is stored in char array. So, how can I achieve this? can you please help me on this.