Skip to main content
vitthal muddapur
Associate III
June 12, 2019
Question

Losses the bytes of data in LPUART IRQ HANDLER?

  • June 12, 2019
  • 3 replies
  • 1188 views

I have configured LPUART with 9600 baud rate and enable receiver interrupt with MCU 65Khz low power mode and my uart handler like

void LPUART1_IRQHandler(void)

{

uint32_t isrflags  = READ_REG(hlpuart1.Instance->ISR);

 uint32_t cr1its   = READ_REG(hlpuart1.Instance->CR1);

 uint32_t errorflags;

 /* If no error occurs */

 errorflags = (isrflags & (uint32_t)(USART_ISR_PE | USART_ISR_FE | USART_ISR_ORE | USART_ISR_NE));

 if (errorflags == RESET)

 {

  /* UART in mode Receiver ---------------------------------------------------*/

  if(((isrflags & USART_ISR_RXNE) != RESET) && ((cr1its & USART_CR1_RXNEIE) != RESET))

  {

 UART_RX_Buffer[UART_Buffer_Counter]=LPUART1->RDR;

  UART_Buffer_Counter++;

if(UART_Buffer_Counter==UART_RX_BUFFER_LENGTH)

UART_Buffer_Counter=0;

   return;

  }

 }

}

and 200ms sytem tick interrupt,

  • Some time losses the uart receiver byte data.
  •  
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
June 12, 2019

Make sure the interrupt grouping/priority is such that this routine preempts others that can run excessively. ie SysTick or others doing a whole bunch on ancillary things.

Don't do any additional processing in the handler beyond filling the buffer.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
vitthal muddapur
Associate III
June 13, 2019

Thank you

When UART communication only Systick interrupt enable with 200ms.

Bob S
Super User
June 12, 2019

So the CPU is running at 65KHz. That means that you have approx 67 CPU clock cycles to respond to each UART interrupt (presuming 8-bit data, no parity which gives 960 bytes/sec). And that includes the exception setup/cleanup and stacking and unstacking registers. Going with what ​ @Community member​ said, and presuming that your ISR uses fewer than that many clock cycles (it looks like it should), then that doesn't leave a whole lot of time for anything else to preempt the LPUART_IRQHandler().