Skip to main content
Visitor II
October 27, 2024
Question

Laptop does not recognize stm32f407g-disc1

  • October 27, 2024
  • 2 replies
  • 842 views

Hello,

I have a Asus Vivobook S15 with Windows 11. I want to connect stm32f407g-disc1 + in my laptop but my laptop does not recognize the device. It is not the problem of the cable nor the device because I used them in other laptops and they get recognized.  then it produces an error and does not recognize the device as part of "USB Devices". The system is updated. I tried to download a drive, a software to upgrade the device but it fails to install. I also turned off the firewall and security temporarily, but it did not work. What can I do in order to make my laptop recognize the device as usb-connected device?

thank you in advance for the help.

    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    October 28, 2024

    Hello @St_user3 ,

    Maybe the problem is with the port of your laptop.

    Did you try upgrade the ST-Link firmware version through : ST-LINK>firmware update or STSW-LINK009.

    Verify that the jumpers on the board are correctly set and that the board is properly powered.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Andrew Neil
    Super User
    October 28, 2024

    Things  to try when the computer is not seeing the ST-Link:

    https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

     


    @St_user3 wrote:

    It is not the problem of the cable nor the device because I used them in other laptops and they get recognized..


    I would still suggest trying other cables - they can be marginal.

    Also check the board very carefully - the connector can become loose/unreliable

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.