2021-11-10 3:11 AM
I am facing an issue with the I2C communication. During the first run the communication between the MCU and the sensor is okay then I can read and write in the sensor's registers without a problem. However, when I try to debug a second time I receive HAL_BUSY when I am trying to communicate with the sensor, the communication is just restablished when the power supply of the board is cut and then fed again.
The Code snippet to write to the register is the following:
HAL_StatusTypeDef MAX30105_WriteRegister(uint8_t reg_addr, uint8_t reg_value){
HAL_StatusTypeDef returnValue = HAL_ERROR;
//Check if the MAX30105 is ready in a trial of 5 times
HAL_StatusTypeDef result = HAL_I2C_IsDeviceReady(&hi2c1, MAX30105_ADDR, 5, 10);
if (result == HAL_OK) // HAL_ERROR or HAL_BUSY or HAL_TIMEOUT
{
returnValue = HAL_I2C_Mem_Write(&hi2c1, MAX30105_ADDR, reg_addr , 1, ®_value, sizeof(reg_value), 10);
if(returnValue != HAL_OK)
return returnValue;
}
return returnValue;
}The I2C setup is:
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}I tried in both boards STM32F407G and STM32F103 Blue Pill.
The sensor is MAX30105 from Maxim.
Is there something that I am missing for the I2C communication that results in such problem?
2021-11-10 4:31 AM
Try a thick power ground wire between the boards,
use 1k pullups, that should help
set the IO pins to Very Fast.
to lower the overall power requirements,
once that is stable, you can lower the pin speed as you tune the IIC IO parameters