Skip to main content
yang hong
Associate III
May 7, 2018
Question

INPUT CAPTURE for timer 3 and timer 13

  • May 7, 2018
  • 7 replies
  • 828 views
Posted on May 07, 2018 at 20:54

Hello, 

I have one input channel for timer. I notice PA6 either for TIM3-CH1 or TIM13-CH1. So it is possible to map pin for both of timers (3 and 13).  if I can do it, how to set them?

Regards,

    This topic has been closed for replies.

    7 replies

    waclawek.jan
    Super User
    May 7, 2018
    Posted on May 07, 2018 at 21:06

    it is possible to map pin for both of timers

    Unless it's a 'F1xx, no.

    JW

    yang hong
    yang hongAuthor
    Associate III
    May 7, 2018
    Posted on May 07, 2018 at 21:10

    I need one input signal for two timers for different task. I am using f429zi. Do you have some suggestion? 

    henry.dick
    Associate II
    May 7, 2018
    Posted on May 07, 2018 at 21:14

    Easy three steps:

    1. Assign two pins, one for each of the two timers.

    2. Wire the two pins together 

    3. Sit back and enjoy your work.