Skip to main content
RSrin
Visitor II
September 20, 2019
Question

In STM32H743zi can HRTIM be used as Time Base generator?

  • September 20, 2019
  • 0 replies
  • 557 views

Hi ,

I need to toggle a GPIO to create a clock pattern for as much as high frequency as possible , So currently using TIM5 and on overflow callback I toggle the GPIO. The generated clock pulse is around 25 us pulse width, I want to decrease pulse width further . Can someone point me to the example where HRTIM can be used to generate time base. Thanks.

This topic has been closed for replies.