IAP failure on writing in STM32f429
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-23 4:54 AM
I am writing a bootloader application that resides in sectors_0 (0x08000000-0x08003FFF) and sector_1 (0x08004000-0x08007FFF) of stm32f429. When the bootloader application starts up it erases sector_2(0x08008000-0x0800BFFF) and sector_3(0x0800C000-0x0800FFFF) of the flash memory. Then loads the main code from an SDCARD and writes it to sector_2 and sector_3.
I can successfully erase sector_2 and sector_3 but when trying to write to them, I get HAL_ERROR.This is the relevant code:/* Unlock the Flash to enable the flash control register access *************/
volatile uint32_t main_addr = 0x08008000;
FLASH_If_Init();
FlashProtection = FLASH_If_GetWriteProtectionStatus();pEraseInit.TypeErase = TYPEERASE_SECTORS;
pEraseInit.Sector = FLASH_SECTOR_2; pEraseInit.NbSectors = 2; pEraseInit.VoltageRange = VOLTAGE_RANGE_3; if (HAL_FLASHEx_Erase(&pEraseInit, &SectorError) != HAL_OK) { /* Error occurred while page erase */ while (1); }if(FLASH_If_Write(main_addr, (uint32_t *)buffer, (fno.fsize)/4)!= FLASHIF_OK) //writes are 32 bit
{ //error while(1);}
Functions being used have been defined in the CUBE project section: STM32Cube\Repository\STM32Cube_FW_F4_V1.21.0\Projects\STM32446E_EVAL :/**
* @brief Unlocks Flash for write access * @param None * @retval None */void FLASH_If_Init(void){ HAL_FLASH_Unlock();/* Clear pending flags (if any) */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGPERR | FLASH_FLAG_PGSERR);}/** * @brief This function writes a data buffer in flash (data are 32-bit aligned). * @note After writing data buffer, the flash content is checked. * @param FlashAddress: start address for writing data buffer * @param Data: pointer on data buffer * @param DataLength: length of data buffer (unit is 32-bit word) * @retval 0: Data successfully written to Flash memory * 1: Error occurred while writing data in Flash memory * 2: Written Data in flash memory is different from expected one */uint32_t FLASH_If_Write(uint32_t FlashAddress, uint32_t* Data ,uint32_t DataLength){ uint32_t i = 0;for (i = 0; (i < DataLength) && (FlashAddress <= (USER_FLASH_END_ADDRESS-4)); i++)
{ /* Device voltage range supposed to be [2.7V to 3.6V], the operation will be done by word */ if (HAL_FLASH_Program(TYPEPROGRAM_WORD, FlashAddress, *(uint32_t*)(Data+i)) == HAL_OK)//<<<<<<<<<This line returns a HAL_ERROR
{ /* Check the written value */ if (*(uint32_t*)FlashAddress != *(uint32_t*)(Data+i)) { /* Flash content doesn't match SRAM content */ return(FLASHIF_WRITINGCTRL_ERROR); } /* Increment FLASH destination address */ FlashAddress += 4; } else { /* Error occurred while writing data in Flash memory */ return (FLASHIF_WRITING_ERROR); } }return (FLASHIF_OK);
}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-23 4:58 AM
Dear
hadez803
‌,what exactly is the issue with IAP?
Please note that sector_0 address is from0x08000000 to0x08003FFF.
Best regards,
Tilen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-23 7:09 AM
Dear
Majerle.Tilen
,I accidentally submitted the question before completing it. I have edited the Question and also fixed the typo about the address of sector_0.
Best Regards