Iam using stm32F4 discovery board to find FFT. But when i use the arm CMSIS library i am getting errors like this
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(160): error: #65: expected a ";"
int32_t lo = (int32_t) ((in << 32) >> 32);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(162): error: #20: identifier "n1" is undefined
n1 = __CLZ(hi) - 32;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(162): error: #20: identifier "hi" is undefined
n1 = __CLZ(hi) - 32;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(168): error: #20: identifier "lo" is undefined
n1 = __CLZ(lo);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(204): error: #20: identifier "lo" is undefined
*normalized = (((uint32_t) lo) >> n1) | (hi << (32 - n1));
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(212): warning: #174-D: expression has no effect
int32_t normalized;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(212): error: #65: expected a ";"
int32_t normalized;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(213): warning: #174-D: expression has no effect
int32_t norm;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(213): error: #65: expected a ";"
int32_t norm;
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(220): error: #20: identifier "normalized" is undefined
arm_norm_64_to_32u(absNum, &normalized, &norm);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/utils.h(220): error: #20: identifier "norm" is undefined
arm_norm_64_to_32u(absNum, &normalized, &norm);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/matrix_functions.h(548): error: #757: function "int32_t" is not a type name
int32_t shift,
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/matrix_functions.h(563): error: #757: function "int32_t" is not a type name
int32_t shift,
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/controller_functions.h(209): error: #757: function "int32_t" is not a type name
int32_t resetStateFlag);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/controller_functions.h(227): error: #757: function "int32_t" is not a type name
int32_t resetStateFlag);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/controller_functions.h(246): error: #757: function "int32_t" is not a type name
int32_t resetStateFlag);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/distance_functions.h(179): error: #757: function "int32_t" is not a type name
float32_t arm_minkowski_distance_f32(const float32_t *pA,const float32_t *pB, int32_t order, uint32_t blockSize);
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(65): error: #757: function "int32_t" is not a type name
__STATIC_INLINE float32_t arm_exponent_f32(float32_t x, int32_t nb)
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(91): error: #757: function "int32_t" is not a type name
const int32_t *classes; /**< The two SVM classes */
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(105): error: #757: function "int32_t" is not a type name
const int32_t *classes; /**< The two SVM classes */
D:\installed\kielpacks\ARM\CMSIS\5.8.0\CMSIS\DSP\Include\dsp/svm_functions.h(106): error: #757: function "int32_t" is not a type name
I have included the path but still iam getting this error