Skip to main content
Associate III
Sep 20, 2024 3:01 AM UTC
Solved

I ran printf over UART but the results were not displayed in Tera Term

 

Hello everyone

I'm using stm32f207ztg6 and want to do printf using UART, but it doesn't show up in Tera Term.
How can I solve this problem?

■ Program used

 

// *-*-*↓main()-*-*-*-*-*-*-*-*-*-*-*-*
setbuf(stdout, NULL);
while (1)
{
/* USER CODE END WHILE */
printf("Hello World\r\n");
HAL_Delay(1000);
/* USER CODE BEGIN 3 */
}
// *-*-*-*-*-*-*-*-*-*-*-*-*-*-*-*-*-*-*

int _write(int file, char *ptr, int len)
{
HAL_UART_Transmit(&huart2,(uint8_t *)ptr,len,10);
return len;
}

static void MX_USART2_UART_Init(void)
{

/* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_W ORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */

/* USER CODE END USART2_Init 2 */

}

 

■STLink: STLink Virtual COM Port

■Situation
When HAL_UART_Transmit is executed, HAL_OK is returned, but nothing is displayed in "Tera Term".

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 20, 2024 3:09 PM UTC

Hello @t-oka ,

First, before starting the printf usage over UART, you need to validate the UART transmission by for example just sending a couple of characters using HAL_UART_Transmit().

Second, you need always to check the schematics or board's user manual before suspecting an issue in the FW.

According to the schematics of MB1137 the UART instance connected to STLink-VCP on NUCLEO-F207ZG (MB1137) is USART3 and not USART2:

SofLit_0-1726844839253.png

So you need to select USART3 instead of USART2

Refer to this printf example. on NUCLEO-F207

Hope it helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

6 replies

mƎALLEm
ST Technical Moderator
Sep 20, 2024 4:22 AM UTC

Hello,

You didn’t tell which board you are using?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
t-okaAuthor
Associate III
Sep 20, 2024 4:41 AM UTC

Hello!
I am using a Nucleo board.

Andrew Neil
Super User
Sep 24, 2024 9:57 AM UTC

@t-oka wrote:

>You should always check the schematic or the board's user manual before suspecting a FW problem.


That's probably the key difference between embedded C (particularly on small microcontrollers), and C on "big" systems (Linux, Windows, et al) - you need to understand the hardware context.

 

See also:

https://community.st.com/t5/stm32-mcus-embedded-software/ds18b20-sensor-detection-via-one-wire-1-wire-protocol/m-p/729960/highlight/true#M55863

 

#HardwareMatters #EssenceOfEmbedded

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.