Skip to main content
KChin.7
Visitor II
May 21, 2019 7:25 AM UTC
Question

I have STEVAL-IDP005V1 and Nucleo64 boards. For the first time, STEVAL-IDP005V1 and Nucleo64 boards are Connected and programmed bin file and got output. But afterwords failed to reprogram STEVAL-IDP005V1 using Nucleo64 board.

Getting Following Error: "There is not enough space on NODE_F070RB. You need an additional 124 KB to copy these files."

    This topic has been closed for replies.

    1 reply

    ETheu.1
    Visitor II
    Mar 13, 2020 8:51 AM UTC

    Hi,

    you'll need to connect the IDP005V1 over the M12 cable to a suitable power source.

    In our case the from ST provided cable had the wrong wire-coloring. So it did not work just by connecting the blue wire to GND and the brown to VDD.