cancel
Showing results for 
Search instead for 
Did you mean: 

How to use NucleoF401 eval Example code without X-nucleo board?

TChap.3
Associate II

I have the X-nucleo VL53L5 board and have modified the example code for a project. Now I need to connect the VL53L5 remotely using my own breakout board that manages its pull-up/down needs. Nucleo only connects scl sda. But the i2c does not run unless X-Nucleo board is on it. What pin/code is checking to be sure the X- is there so I can turn it off? This code will get ported to smaller F401 “pill�? with only scl sda.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TChap.3
Associate II

The person working on the code for me told me it was not the code. It was a board issue not letting the STM boot up without a board attached.

TChap.3
Associate II

“these seems to work. Add a pull-up between 3.3V and NRST, or short these two pins�?.